Home Technologies Electromechanical Group Electromechanical Knowledge Base What should I replace my S Drive with? S6, S8 or S3
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base What should I replace my S Drive with? S6, S8 or S3
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX+
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives-
      • At what voltage does the SX regen circuit turn on?
      • Can the SX be converted to an S drive?
      • How can I end an SX error routine?
      • L20 with S and ZETA Series drives
      • Maximum AC voltage for the SX drive
      • Replacement Batteries & Installation Instructions
      • S/SX Drives: Connector Part Numbers
      • S3 / SX3 / SXF3 DIP Switches and Dimensions
      • SX Error Code:
      • SX Error---Battery Backup Ram Corrupted
      • SX is not Compatible with the AR-23
      • SX Kill Sequence
      • SX OPHV pullups
      • SX Registration and TDR Command
      • SX8 Fan Current Draw
      • What replaces a 87-011279-01B? 87-011751-01E?
      • What replaces a SX drive?
      • What should I replace my S Drive with? S6, S8 or S3
      • X-WARE 5.1 Tutorial
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
What should I replace my S Drive with? S6, S8 or S3

Print Friendly and PDF

Note the S drives are no longer repairable. We recommend the ZETA family of microstepping drives to replace the obsolete S family of microstepping drives. Conversion details are listed below.

S3-Drive can be replaced by the ZETA4 or E-AC drive.

S6-Drive can be replaced by the ZETA4 Drive, E-AC or the ZETA8 Drive depending on the actual current levels being used. Check your S Drive DIP switch settings to determine the current level being used. Below is a chart listing the current levels for the S motors, commonly used with the S/SX.

The ZETA4 is rated up to 4 Amps while the ZETA8 is rated up to 8 Amps. The E-AC is rated up to 3.5 Amps. The S6 was rated up to 6 Amps.

S8-Drive can be replaced by the ZETA8 Drive.

S series Systems

S drives were also sold with S motors as systems. Example, S57-51 included a S6 drive and a S57-51 motor. The S motors are still available with -MO (motor only) designator. Example:  S57-51-MO    The motors in these systems were always in series. However, the customer could change the wiring and dipswitches. In that case, ZETA8 may be needed instead of the ZETA4 or E-AC.

Recommended replacements listed below:

S System Drive P/N Motor P/N
S57-51 ZETA4 or E-AC ZETA57-51-MO
S57-51-E ZETA4 or E-AC ZETA57-51-MO-E
S57-83 ZETA4 or E-AC ZETA57-83-MO
S57-83-E ZETA4 or E-AC ZETA57-83-MO-E
S57-102 ZETA4 or E-AC ZETA57-102-MO
S57-102-E ZETA4 or E-AC ZETA57-102-MO-E
S83-62 ZETA4 or E-AC ZETA83-62-MO
S83-62-E ZETA4 or E-AC ZETA83-62-MO-E
S83-93 ZETA4 or E-AC ZETA83-93-MO
S83-93-E ZETA4 or E-AC ZETA83-93-MO-E
S83-135 ZETA4 or E-AC ZETA83-135-MO
S83-135-E ZETA4 or E-AC ZETA83-135-MO-E
S106-178 ZETA8 N/A*
S106-178-E ZETA8 N/A*
S106-205 ZETA8 S106-205-MO
S106-205-E ZETA8 S106-205-MO-E
S106-250 ZETA8 N/A*
S106-250-E ZETA8 N/A*

 

Dimensions

The ZETA4 is shorter and shallower (depth) and thinner than the S3, S6, or S8 drives were. The mounting foot print is thus also different (smaller). Refer to the user documentation for exact dimensions.

The ZETA8 is roughly the same height and depth as the S3, S6, or S8 drives were. The width is much less than the S8 Drive or the S6 Drive w/ optional fan kit installed was. The mounting footprint is different than the S Drives so that will need to be adjusted for.

Note - The ZETA family does not provide for the 'side-mount' option that the S family allowed by relocating the S Drive mounting tabs. The ZETA family mounting tabs are not relocatable so cabinet depth could be an issue if the 'side-mount' option was used with your S Drive.

Connections

The indexer connections are the same on the S Drive as on the ZETA and E-AC drives. They each use a 25 pin D Sub style connector and the same pin-out for the basic control signals.

Note - The S Drive also had a 'Zero Phase' input available on its indexer connector. The ZETA Drives do not provide a 'Zero Phase' input. Rather these same pins provide a 'Reset' input instead. Standard Parker (Compumoor) cables and indexers did not make use of either of these input features.

The ZETA4 has the same motor connector as the S3 and S6 drives had, a 9 pin screw terminal. Your existing motor cable/connector can be re-used as is.

The ZETA8 has the same motor connector as the S8 drives had, a 7 pin screw terminal. Your existing motor cable/connector can be re-used as is.

Note - S8 Drives built prior to Nov 6, 1995 used the smaller gauge 9 pin screw terminal but was changed to the larger gauge 7 pin screw terminal after this date. If your S8 uses the 9 pin connector then you will need to re-wire the motor cable to the ZETA8 larger 7 pin connector as shown in the ZETA user guides.

Power

The ZETA4 and ZETA8 drive operate from the same 120VAC input supply as the S3, S6, or S8 would have used.

The E-AC uses screw terminals for the 120VAC input.

Settings

The ZETA family is configured via DIP switch settings in a similar fashion to the S family drives were. There is not a one-to-one correlation in settings so you will need to compare the existing S Drive DIP settings and transfer those to the corresponding ZETA DIP settings.

S Drive to Zeta Drive DIP Switch Crossover Sheet

The E-AC uses microswtiches internal to set the current level. Remove the cover to set before connecting motor.

E-AC Quick Reference guide

Motors

The S57 (Nema 23) and S83 (Nema 34) frame step motors are the exact same motors as the ZETA57 and ZETA83 frame motors, simply re-released under the ZETA family name. The S106 (Nema 42) frame motors were not carried to the ZETA family but are compatible with the ZETA8 drives. Check the existing S Drive DIP settings and transfer to the corresponding ZETA DIP settings.

These motors are also the same as the ES series step motors, however with those, no connector is provided at the end of the cable (as these are provided with the drives).

S User Guides

ZETA User Guides

 

 

 

CP*S6-DO-125VDC
CP*S6-DRIVE-10010
CP*S6-DRIVE-10031
CP*S6-DRIVE-10065
CP*S6-DRIVE-10452
CP*S6-DRIVE-10748
CP*S6-DRIVE-9655
CP*S6-DRIVE-RES
CP*S8-DRIVE
CP*S8-DRIVE-10018
CP*S8-DRIVE-10065
CP*S8-DRIVE-10747
CP*S8-DRIVE-9730
CP*S8-DRIVE-9979
CP*S-DRIVE
MODEL S6-DRIVE
MODEL S6-DRIVE-R
MODEL S8-DRIVE
MODEL S8-DRIVE-R
MODEL SX6-DRIVE
MODEL SX6-DRIVE-R
MODEL SX8-DRIVE
MODEL SX8-DRIVE-R
MODEL SXF6-DRIVE
MODEL SXF8-DRIVE
S106-178
S106-178-E
S106-178-MO
S106-178-MO-E
S106-178-MO-R
S106-178-MO-S
S106-178-S
S106-205
S106-205-E
S106-205-MO
S106-205-MO-E
S106-205-MO-ETM
S106-205-MO-R
S106-205-MO-S
S106-205-S
S106-250
S106-250-E
S106-250-MO
S106-250-MO-E
S106-250-MO-R
S106-250-MO-S
S106-250-S

S3
S3-57-102
S3-57-102-PR
S3-57-51
S3-57-83
S3-83-62-PR
S3-DRIVE
S3-DRIVE-PR
S3-ETM
S57-102-MO
S57-102-MO-DEMO
S57-102-MO-E
S57-102-MO-F
S57-102-MO-R
S57-102-MO-S
S57-102-S
S57-51
S57-51-E
S57-51-MO
S57-51-MO-DEMO
S57-51-MO-E
S57-51-MO-E-ETM
S57-51-MO-F
S57-51-MO-R
S57-51-MO-S
S57-51-MO-S-R
S57-51-NSK
S57-51-R
S57-51-S
S57-83
S57-83-E
S57-83-MO
S57-83-MO-DEMO
S57-83-MO-E
S57-83-MO-E-R
S57-83-MO-F
S57-83-MO-R
S57-83-MO-S
S57-83-NSK
S57-83-S
S83-135
S83-135-E
S83-135-MO
S83-135-MO-E
S83-135-MO-E-ETM
S83-135-MO-ETM
S83-135-MO-F
S83-135-MO-K
S83-135-MO-R
S83-135-MO-S
S83-135-MO-S-F
S83-135-MO-S-K
S83-135-S
S83-62
S83-62-E
S83-62-MO
S83-62-MO-E
S83-62-MO-ETM
S83-62-MO-R
S83-62-MO-S
S83-62-R
S83-62-S
S83-93
S83-93-E
S83-93-MO
S83-93-MO-DEMO
S83-93-MO-E
S83-93-MO-E-DEMO
S83-93-MO-F
S83-93-MO-R
S83-93-MO-S
S83-93-R
S83-93-S

S6-DRIVE
S6-DRIVE-BETA
S6-DRIVE-R
S8-AMP-BETA
S8-DRIVE
S8-DRIVE-AMP INC.
S8-DRIVE-AMP-V2
S8-DRIVE-AMP-V2-1
S8-DRIVE-BETA
S8-DRIVE-DEMO
S8-DRIVE-ETM
S8-DRIVE-R
S8-DRIVE-REP
SX106-178
SX106-178-A
SX106-178-E
SX106-178-R
SX106-178-S
SX106-205
SX106-205-A
SX106-205-E
SX106-205-S
SX106-250
SX106-250-A
SX106-250-E
SX106-250-S
SX3-57-102-PR
SX3-57-51
SX3-57-51-PR
SX3-83-135-PR
SX3-83-62-PR
SX3-83-93-PR
SX3-DRIVE
SX3-DRIVE-DEMO
SX3-DRIVE-PR
SX57-102
SX57-102-A
SX57-102-E
SX57-102-S
SX57-51
SX57-51-A
SX57-51-E
SX57-51-S
SX57-83
SX57-83-A
SX57-83-E
SX57-83-S
SX6 SHIPKIT
SX6-DRIVE
SX6-DRIVE-A
SX6-DRIVE-A-R
SX6-DRIVE-A-RED
SX6-DRIVE-BETA
SX6-DRIVE-ETM
SX6-DRIVE-R
SX6-DRIVE-RED
SX8 SHIPKIT
SX83-135
SX83-135-A
SX83-135-E
SX83-135-R
SX83-135-S
SX83-62
SX83-62-A
SX83-62-E
SX83-62-S
SX83-62-S-R
SX83-93
SX83-93-A
SX83-93-E
SX83-93-S
SX8-DRIVE
SX8-DRIVE-A
SX8-DRIVE-A-RED
SX8-DRIVE-BETA
SX8-DRIVE-ETM
SX8-DRIVE-R
SX8-DRIVE-RED
SX8-DRIVE-R-ETM
SX-DEMO-BOX
SXF KIT
SXF106-178
SXF106-178-E
SXF106-205
SXF106-250
SXF106-250-E
SXF3-57-83
SXF3-DRIVE
SXF57-102
SXF57-102-A
SXF57-51
SXF57-51-E
SXF57-83
SXF6-DRIVE
SXF6-DRIVE-A
SXF6-DRIVE-R
SXF83-135
SXF83-135-E
SXF83-62
SXF83-93
SXF83-93-E
SXF8-DRIVE
SXF8-DRIVE-R

glh 10/9/12

1/10/16jh part numbers added
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.