Home Technologies Electromechanical Group Electromechanical Knowledge Base PC Card Controllers (Discontinued)
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base PC Card Controllers (Discontinued)
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)-
        • ACR Controller Fuses
        • ACR Controllers: Connector Part Numbers
        • ACR1000 Support
        • Drive Enable differences: 9000 vs Bus-Based
        • Replace obsolete controllers
        • Unable to re-connect to ACR ...
        • Upgrading from ACR8020 to ACR9000 Part1
        • Upgrading from ACR8020 to ACR9000 Part2
        • ACR controller cards that do not have 64 I/O
        • ACR Controller Communication Performance
        • ACR controller require stable voltage
        • ACR to Compumotor drives -- Resistor packs
        • ACR1500 Connection To PLC
        • ACR1505 and ACR1500 Opto boards
        • ACR2000 Green LED blinks ON and OFF
        • ACR8020 driver OS supported
        • ACR8020 Expansion
        • ACR8020 requres 3.3VDC and 5VDC
        • ACR8020/1505 with MS-DOS applications
        • ACR8K WinNT driver with NT real-time extensions.
        • AcroLib Samples
        • Acroloop with Linux
        • Acromill and Acrocut for DOS Memory Requirements
        • Acroview Alias Names In PLC Programs
        • Analog output(s) stuck at -1.3VDC
        • Battery for the ACR1200, ACR8010, and ACR2000PS
        • Can I use Windows ME to run my Acroloop cards?
        • Can older firmwares be loaded onto a ACR2000?
        • Comm Error 6 using Win NT
        • Configuring for Open loop stepper
        • Connector Part Numbers - RBC, RBD
        • Encoder gate array update
        • Encoder with external power
        • Error 31 Bad Flowfile encontered
        • Error Message 7 in event log
        • Field replacement of the ACR8010
        • Firmware upgrade for ACR8000 Controller
        • Firmware Version 1.18.04 to 1.18.06
        • Firmware Version 1.18.06 to 1.18.07
        • How do I disconnect from an ACR controller?
        • How do I use the ACRXPC.OCX control?
        • Intelligent I/O Controller
        • Is ACROWNT.DLL compatible with .NET?
        • ISA-based controller addresses
        • Kill All Moves and
        • Legacy Product Page - Acroloop Controllers
        • Locating version of the PCI Driver
        • Multiple PCI cards in a PC
        • New 8010 has red lights on startup
        • NT Service Pack 6 Users
        • OPS8000 programming
        • Porting programs from ACR2000 to ACR1500
        • Reboot causes loss of communication (Error -16)
        • Replacing ACR ISA bus controller with ACR8020
        • Sinking/Sourcing Digital I/O
        • Static Sensitive
        • System log messages are not descriptive
        • Transferring Files in Acroview
        • Transferring Position Information
        • Upgrading from ACR1500 to ACR1505
        • Use of a Null Modem cable.
        • Using ACROWNT.DLL with Borland C++
        • Using serial communication
        • Using the Acroloop toolset with Borland C++
        • Watchdog relay function
        • What is needed for the ACR autobaud process?
        • Windows 98 and Backpack-style CD-ROM drives
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
PC Card Controllers (Discontinued)

Print Friendly and PDF

PC Card Controllers

  • ACR Controller Fuses
  • ACR Controllers: Connector Part Numbers
  • ACR1000 Support
  • Drive Enable differences: 9000 vs Bus-Based
  • Replace obsolete controllers
  • Unable to re-connect to ACR ...
  • Upgrading from ACR8020 to ACR9000 Part1
  • Upgrading from ACR8020 to ACR9000 Part2
  • ACR controller cards that do not have 64 I/O
  • ACR Controller Communication Performance
  • ACR controller require stable voltage
  • ACR to Compumotor drives -- Resistor packs
  • ACR1500 Connection To PLC
  • ACR1505 and ACR1500 Opto boards
  • ACR2000 Green LED blinks ON and OFF
  • ACR8020 driver OS supported
  • ACR8020 Expansion
  • ACR8020 requres 3.3VDC and 5VDC
  • ACR8020/1505 with MS-DOS applications
  • ACR8K WinNT driver with NT real-time extensions.
  • AcroLib Samples
  • Acroloop with Linux
  • Acromill and Acrocut for DOS Memory Requirements
  • Acroview Alias Names In PLC Programs
  • Analog output(s) stuck at -1.3VDC
  • Battery for the ACR1200, ACR8010, and ACR2000PS
  • Can I use Windows ME to run my Acroloop cards?
  • Can older firmwares be loaded onto a ACR2000?
  • Comm Error 6 using Win NT
  • Configuring for Open loop stepper
  • Connector Part Numbers - RBC, RBD
  • Encoder gate array update
  • Encoder with external power
  • Error 31 Bad Flowfile encontered
  • Error Message 7 in event log
  • Field replacement of the ACR8010
  • Firmware upgrade for ACR8000 Controller
  • Firmware Version 1.18.04 to 1.18.06
  • Firmware Version 1.18.06 to 1.18.07
  • How do I disconnect from an ACR controller?
  • How do I use the ACRXPC.OCX control?
  • Intelligent I/O Controller
  • Is ACROWNT.DLL compatible with .NET?
  • ISA-based controller addresses
  • Kill All Moves and
  • Legacy Product Page - Acroloop Controllers
  • Locating version of the PCI Driver
  • Multiple PCI cards in a PC
  • New 8010 has red lights on startup
  • NT Service Pack 6 Users
  • OPS8000 programming
  • Porting programs from ACR2000 to ACR1500
  • Reboot causes loss of communication (Error -16)
  • Replacing ACR ISA bus controller with ACR8020
  • Sinking/Sourcing Digital I/O
  • Static Sensitive
  • System log messages are not descriptive
  • Transferring Files in Acroview
  • Transferring Position Information
  • Upgrading from ACR1500 to ACR1505
  • Use of a Null Modem cable.
  • Using ACROWNT.DLL with Borland C++
  • Using serial communication
  • Using the Acroloop toolset with Borland C++
  • Watchdog relay function
  • What is needed for the ACR autobaud process?
  • Windows 98 and Backpack-style CD-ROM drives
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.