Home Technologies Electromechanical Group Electromechanical Knowledge Base General - Unipolar and Bipolar motors.
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base General - Unipolar and Bipolar motors.
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • Step Motors-
    • A/AX Motors - A vs M motors
    • eCLM Motors - Stepper motor Resonant speeds
    • General - Checking Stepper Motor Phases.
    • General - Connectors on Step Motor Cables?
    • General - Custom Stepper Motors
    • General - Encoder Option Clarification for Step Motors (-EC or -E options )
    • General - How many steps per revolution do our motors have?
    • General - Operating Temperature Range for Stepper Motors
    • General - Series vs Parallel wiring in motors
    • General - Step Drive and Motor Compatibility Chart (older legacy lines)
    • General - Stepper Cross-Over Chart (discontinued models)
    • General - Stepper Motor Fault.
    • General - Steppers: Determining Pinouts
    • General - Unipolar and Bipolar motors.
    • General - Unipolar Drive Wiring with Bipolar Motors
    • General - Why is my stepper motor getting hot?
    • LV/HV Motors - Customs
    • LV/HV Motors - HV and LV 34 Frame Stepper Motor Round Shaft Option
    • LV/HV Motors - IP rating on stepper motors?
    • LV/HV Motors - Purple or Red/White Wire
    • LV/HV Motors - Replacements for the VS series step motors
    • LV/HV Motors - Step Motor Wiring
    • LV/HV Motors - Stepper Motor Order Code
    • LV/HV Motors - Stepper motor Resonant speeds (Waveform, Balance, Offset)
    • OEM Motors - Connector Part Numbers
    • OEM Motors - OEM Step Motor Part Numbers
    • PK Motors - PK162-308 Specifications
    • Replacing S106 or TS41 TS42 TS43 step motors with Servo Motors
    • S/SX Motors - Motor inductance
    • S/SX Motors - Replacing S/ZETA/ES series step motors with BE servo motors
    • S/SX Motors - S106 Motor Replacements
    • S/SX Motors - S106 motor specifications
    • S/SX Motors - Step motors with Brad Harrison Connectors (Yellow 5 pin)
    • VS Motors - Motor Cables
    • VS Motors - Wiring and Currents
    • ZETA, S, ES Series Step Motors Discontinued & Suggested Replacements
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
General - Unipolar and Bipolar motors.

Print Friendly and PDF

Some drives were designed to use unipolar motors. Others use bipolar motors. Unipolar motors with 5-leads cannot be used on Bipolar drives. Bipolar motors with 8-leads can be used on Unipolar drives. Some Bipolar motors with 6-leads can be used on Unipolar drives.

To easiest way to wire an 8-lead motor for a Unipolar configuration is to first wire it in a Series configuration. This creates two centertaps: an A-centertap and a B-centertap. To complete the Unipolar configuration, those two centertaps are tied together to create V+. The four remaining wires are A+, A-, B+, and B-.

CAUTION: The current used with an 8-lead motor wired in a Unipolar configuration should be 0.707 times the rated current for that motor in a Series configuration.

The amount of current allowed through the windings is limited by thermal considerations. Only so much heat can go into the motor before it melts. A motor has two halves to a winding: A+ to A-centertap and A-centertap to A-. Let's say that each half has a resistance of 10 Ohms. The current in a Unipolar drive flows from the A-centertap to either of the A+ or the A-, but only one at a time. Let's say the drive is providing 1 Amp. That 1 Amp only flows through half the winding, which is 10 Ohms. The power lost that heats the motor is P=I^2*R or P = 10W. Using the same motor on a bipolar drive where the current flows from A+ to A-, the current needs to be derated by 0.707. By derating, P=(0.707^2) * (2 * 10 Ohm) = 10W. The motor sees the same amount of power running through it with both methods.
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.