Home Technologies Electromechanical Group Electromechanical Knowledge Base Clear all memory in an ACR controller
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base Clear all memory in an ACR controller
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
Clear all memory in an ACR controller

Print Friendly and PDF

Performing a Return to Factory settings or clearing the memory on a ACR card requires the following steps to be entered at the "SYS>" prompt.

For the ACR7000, ACR9000, ACR9030, ACR9040 or PAC ACR9600, ACR9630 or ACR9640

1. FLASH RES

This command returns the controller to factory settings.
Performs the following actions:

  • Clears all memory dimensioned for programs, variable, arrays, and data logging
  • Resets the communication stream dimensions
  • Erases all system parameters
  • Erases user images from flash memory
  • Resets the hardware configuration
  • Cycles power to the controller
  • Resets ip address to default (192.168.10.40 subnet 255.255.255.0)
  • ACR7000 default ip address (192.168.100.1 subnet 255.255.255.0)



For the IPA or AriesCE

1. FLASH RES

Command returns the controller to factory settings.
Performs the following actions:
Erases motor configuration and user programs (ERASE + FLASH ERASE)

Resets IP address to default (set via rotary dial switches) (192.168.100.x subnet 255.255.255.0,  where x is the rotary switch value)




For the ACR8020 and ACR1505

1. HALT ALL
2. NEW ALL
3. DETACH ALL
4. CLEAR
5. ERASE
6. FLASH ERASE
7. CONFIG CLEAR
8. CLEAR DPCB
9. CLEAR COM1
10. CLEAR COM2
11. BRESET
12. REBOOT

For the ACR1200, ACR1500, ACR2000, ACR8010

1. HALT ALL
2. NEW ALL
3. DETACH ALL
4. CLEAR
5. ERASE
6. FLASH ERASE
7. CONFIG CLEAR
8. CLEAR FIFO
9. CLEAR COM1
10. CLEAR COM2
11. BRESET
12. REBOOT
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.