Home Technologies Electromechanical Group Electromechanical Knowledge Base General - Why is my stepper motor getting hot?
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base General - Why is my stepper motor getting hot?
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • Step Motors-
    • A/AX Motors - A vs M motors
    • eCLM Motors - Stepper motor Resonant speeds
    • General - Checking Stepper Motor Phases.
    • General - Connectors on Step Motor Cables?
    • General - Custom Stepper Motors
    • General - Encoder Option Clarification for Step Motors (-EC or -E options )
    • General - How many steps per revolution do our motors have?
    • General - Operating Temperature Range for Stepper Motors
    • General - Series vs Parallel wiring in motors
    • General - Step Drive and Motor Compatibility Chart (older legacy lines)
    • General - Stepper Cross-Over Chart (discontinued models)
    • General - Stepper Motor Fault.
    • General - Steppers: Determining Pinouts
    • General - Unipolar and Bipolar motors.
    • General - Unipolar Drive Wiring with Bipolar Motors
    • General - Why is my stepper motor getting hot?
    • LV/HV Motors - Customs
    • LV/HV Motors - HV and LV 34 Frame Stepper Motor Round Shaft Option
    • LV/HV Motors - IP rating on stepper motors?
    • LV/HV Motors - Purple or Red/White Wire
    • LV/HV Motors - Replacements for the VS series step motors
    • LV/HV Motors - Step Motor Wiring
    • LV/HV Motors - Stepper Motor Order Code
    • LV/HV Motors - Stepper motor Resonant speeds (Waveform, Balance, Offset)
    • OEM Motors - Connector Part Numbers
    • OEM Motors - OEM Step Motor Part Numbers
    • PK Motors - PK162-308 Specifications
    • Replacing S106 or TS41 TS42 TS43 step motors with Servo Motors
    • S/SX Motors - Motor inductance
    • S/SX Motors - Replacing S/ZETA/ES series step motors with BE servo motors
    • S/SX Motors - S106 Motor Replacements
    • S/SX Motors - S106 motor specifications
    • S/SX Motors - Step motors with Brad Harrison Connectors (Yellow 5 pin)
    • VS Motors - Motor Cables
    • VS Motors - Wiring and Currents
    • ZETA, S, ES Series Step Motors Discontinued & Suggested Replacements
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
General - Why is my stepper motor getting hot?

Print Friendly and PDF

Stepper motors do get hot. Their cases can get up to about 100 - 110 degrees C. This is because the drive is supplying the motor with full current the whole time to keep the motor in position. (This is different than a servo where the drive only gives the servo motor as much current needed to maintain its postion. The servo has feedback for this purpose where the stepper does not.)

If you run a stepper motor on a desktop without a heatsink, depending on how much current the drive is setup to put into the motor, the motor is in danger of being burned up.

There are several ways to reduce the temperature that a stepper motor can get up to...

1) Mount the motor to a proper heatsink. What the motor mounts to makes a big difference. A gearbox does not make a good heatsink. Neither does a mounting plate that is the same size as the motor's mounting flange. The temperature difference of a stepper motor on and off of a heatsink can be up to 40 degrees C!

What is a good heat sink?
23 frame: 6-inch x 6-inch x .5-inch
10-inch x 10-inch x 0.25-inch aluminium heatsink2) Use the drive's current reduction ability if it has it. Parker's stepper drives all have some sort of current reduction ability that reduces the amount of current supplied to the drive when the motor is at a standstill. This works on horizontal loads without any external forces. When this function is used vertical loads could fall with ballscrews, belts or low friction systems with applied loads that are constantly trying to backdrive the motor. As step motors have higher torque at low speeds and less torque is required to hold a load than accelerate a load, whether a step motor will back drive in a current foldback condition depends on the system friction and loads. Leadscrews are typically self-locking or a brake on a ballscrew and would better choices.

3) Make sure their is plenty of airflow. A stepper motor in a tight and confined space will not be able to shed its heat. Using good air circulation and a fan will help the motor to dissipate the heat that it builds up.

More information on choosing a step motor and how motor current settings are chosen.

Related FAQ:
Stepper Motor Current Settings
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.