Home Technologies Electromechanical Group Electromechanical Knowledge Base PDS Replacement
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base PDS Replacement
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • Legacy (Discontinued)-
    • 4000+
    • Compax and SV+
    • 6000+
    • APEX & APEX615x+
    • BLOK+
    • Compucam+
    • Digiplan BD, BDS, BDHX,BL, BLX,BLHX, PDS, PDX, PDHX-
      • Battery for the PDX &TQ10X Drive
      • Battery Replacement for BDHX,BLX,BLHX,PDHX, X150
      • BL, BLX, BLH, BLHX, ML Suggested Replacements
      • BLHX Error
      • BLHX Error #25
      • BLHX Part Number
      • BLHX Registration Speed
      • BLX Outputs.
      • Can I use a ML motor in place of a MD motor?
      • Error code 3 - Memory map changed
      • Establishing Communication with the PDX
      • No Communication with the BDHX?
      • No motion? Check motor resolution for the PDX
      • PDHX-E Troubleshooting Codes.
      • PDHX15E Self Test
      • PDS Power Dump Option(-D)
      • PDS Replacement
      • PDS13 PDS15 PDX13 PDX15 Connector Part Numbers
      • PDX Replacement
      • Removal of RS485 in PDHX-E and BDHX-E
    • iBE+
    • 630 Family Replacement Options (631, 635, 637) (Parker SSD / Eurotherm out of Europe)
    • L20+
    • MP-FLX and FLX+
    • MPA Servo Drives+
    • Motion Architect+
    • PC21+
    • RP240+
    • S/SX Drives+
    • OEM Products+
    • SFD Servo Drives and SF Servo Motors+
    • SLVD & HPD+
    • TBF & TBN Servo Drives+
    • TQ10 & TQ10X+
    • XWare / X Language+
    • Z ZX ZXF Drives+
    • Downloading from the FTP site
    • MTS Automation / Custom Servo Motor User Guides and Documentation Location
    • Retired Products
    • Torque, Velocity & Position Loops
    • Legacy Product Page - Luge LM Series
    • Parvex Motion Explorer and Easy Rider Software
    • Running the SMA with a DC Brushed Motor
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
PDS Replacement

Print Friendly and PDF
The OEM750 is a very good possibility for replacing the PDS. They have the same basic capabilities, but there are a few hardware differences:

(The ZETA4, E-AC and ViX-IM are also options for replacing the PDS.)

POWER SUPPLY: The PDS took 110 and 240 Volts AC input. The OEM750 requires an external 24 - 75 VDC power supply. The OEM300 and OEM1000 both supply 75 VDC and can both take 120 and 240 VAC.

The ViX-IM requires a separate power supply that provides both 24 VDC for logic and 80 VDC or less for drive power.

The ZETA4 and E-AC are other alternatives that take 120VAC. The ZETA4-240 takes 240VAC.

BUS VOLTAGE: This directly affects the speed capability of the motor. The PDS's bus voltage was 70 VDC. The OEM750's bus voltage depends on the DC voltage being put into it; whatever DC voltage is put in is the bus voltage for the OEM750. Using an OEM300 which puts 75 VDC into the OEM750 will provide just slightly more performance than the PDS could. Likewise, using a different power supply that only puts 24 VDC into the OEM750 will make the OEM750 provide much LESS performance than the PDS could.

The bus voltage for the ViX-IM is 80VDC or less based on the external power supply.

The bus voltage for the ZETA4 and E-AC are both 170VDC. Some motors cannot be used with a bus voltage this high. Most of the motors used with the PDS can handle it. For example, the PDS-57-51 motor can be used with the ZETA4.
MOTOR RESOLUTION SETTING: The PDS had a default and maximum drive resolution of 4,000 steps/revolution. The OEM750 doesn't have that 4,000 setting. It does have 2,000 and 5,000. This will effect how many pulses are needed on the Step input to turn the motor one revolution.

The ViX-IM can have its drive resolution set to 4,000.

The ZETA4 and E-AC also do not have a 4,000 count resolution setting.

INTERNAL OSCILLATOR: The PDS had an internal oscillator that would allow a jog functionality with a potentiometer and an input without the need for an exteranl command signal. To replace this functionality, a drive with an indexer would be needed so that the jog functionality could be programmed. The OEM750X-M2 and ViX are both possible products for this type of functionality.

The E-AC with some custom functionality is also a possibility. Please see the FAQ for the E-AC titled "Can I get some level of control on the E-AC?"

Note: The PDSxx and PDSxx-2's are the same. Digiplan dropped the -2 on later models. So, a PDS13-2 and PDS13 are the same. The PDS15-2 and the PDS15 are the same. The /US designation does not signify a hardware change; only that it was originally sold from Parker Compumotor in the US.
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.