Home Technologies Electromechanical Group Electromechanical Knowledge Base General - How many steps per revolution do our motors have?
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base General - How many steps per revolution do our motors have?
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
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
  • Step Motors-
    • A/AX Motors - A vs M motors
    • eCLM Motors - Stepper motor Resonant speeds
    • General - Checking Stepper Motor Phases.
    • General - Connectors on Step Motor Cables?
    • General - Custom Stepper Motors
    • General - Encoder Option Clarification for Step Motors (-EC or -E options )
    • General - How many steps per revolution do our motors have?
    • General - Operating Temperature Range for Stepper Motors
    • General - Series vs Parallel wiring in motors
    • General - Step Drive and Motor Compatibility Chart (older legacy lines)
    • General - Stepper Cross-Over Chart (discontinued models)
    • General - Stepper Motor Fault.
    • General - Steppers: Determining Pinouts
    • General - Unipolar and Bipolar motors.
    • General - Unipolar Drive Wiring with Bipolar Motors
    • General - Why is my stepper motor getting hot?
    • LV/HV Motors - Customs
    • LV/HV Motors - HV and LV 34 Frame Stepper Motor Round Shaft Option
    • LV/HV Motors - IP rating on stepper motors?
    • LV/HV Motors - Purple or Red/White Wire
    • LV/HV Motors - Replacements for the VS series step motors
    • LV/HV Motors - Step Motor Wiring
    • LV/HV Motors - Stepper Motor Order Code
    • LV/HV Motors - Stepper motor Resonant speeds (Waveform, Balance, Offset)
    • OEM Motors - Connector Part Numbers
    • OEM Motors - OEM Step Motor Part Numbers
    • PK Motors - PK162-308 Specifications
    • Replacing S106 or TS41 TS42 TS43 step motors with Servo Motors
    • S/SX Motors - Motor inductance
    • S/SX Motors - Replacing S/ZETA/ES series step motors with BE servo motors
    • S/SX Motors - S106 Motor Replacements
    • S/SX Motors - S106 motor specifications
    • S/SX Motors - Step motors with Brad Harrison Connectors (Yellow 5 pin)
    • VS Motors - Motor Cables
    • VS Motors - Wiring and Currents
    • ZETA, S, ES Series Step Motors Discontinued & Suggested Replacements
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
General - How many steps per revolution do our motors have?

Print Friendly and PDF

All Parker's stepper motors are built with 50 pole pairs, resulting in 200 physical steps per revolution. But by using Parker's microstepping technology (included on all stepper drives), you can actually get 25000 steps or more per rev. The maximum number of steps/rev really depends on the drive.


Gemini (GT/GT6/GT6K): 128000
Vix IM: 51200
Zeta / OEMZL: 50800
E-AC / E-DC: 50800
OEM750/750X: 50800
OEM650/650X: 50800 (also applies to the OEM350/350X)
S/SX: 50800
Integral E: 36000
PDS/PDX: 4000
What effect does resolution have?

When the drive receives step pulses from its indexer (a.k.a. controller), it turns the motor that many steps. However, the size of each "step" is decided by the drive's Resolution setting.
Higher resolutions mean that the drive will make the motor take smaller steps. So, if two drives receive the same number of steps from an indexer, the drive with the higher resolution will spin its motor slower, and not as far, as the drive with the smaller resolution.

The higher the resolution, the more precisely the indexer can position the motor. With a resolution of 50,000 steps/rev, the motor can be positioned at any one of 50,000 different places! This is equivalent to 0.0072 degrees.

Full-stepping is when the drive turns the motor one full physical step (1/200 of a revolution) per indexer step that it receives. Half-stepping means each step is half as big, so the motor will need twice as many steps to go 1 revolution.

With microstepping, we can control the motor with much greater precision, making it take extremely tiny steps. Microstepping a motor also improves smoothness and greatly helps to reduce resonance. There is a slight reduction in torque as compared with full-stepping.
No matter what resolution a drive is set to, the smallest increment the motor can actually turn, from start to finish, is about 0.1 degrees. (This is the amount necessary to overcome friction.) Of course, you can turn the motor forward 0.5 degrees, and then backward 0.495 degrees!

  • motor
  • revolution
  • Step
  • Resolution
  • many
  • stepper
  • steps
  • number
  • Parker
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.