Home Technologies Electromechanical Group Electromechanical Knowledge Base How to Calculate the Gear Offset Parameter?
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base How to Calculate the Gear Offset Parameter?
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
How to Calculate the Gear Offset Parameter?

Print Friendly and PDF
When calculating the GEAR OFFSET PARAMETER P12296, P12552, etc. There are four values that need to be known. There is the source count or source value, the GEAR PPU, the GEAR RATIO and the PPU for the AXIS. The equation to calculate the GEAR OFFSET PARAMETER is shown below.

(Source Count)/ GEAR PPU = Value1
Value1 * GEAR RATIO = Value2
Value2 * PPU AXIS = GEAR OFFSET PARAMETER

Attached a sample code utilizing the ratch feature:

PROGRAM
PBOOT

REM ATTACH MASTER AND SLAVES
ATTACH MASTER 0
ATTACH SLAVE0 AXIS0 "X"
ATTACH AXIS0 STEPPER0 STEPPER0
ATTACH SLAVE1 AXIS1 "Y"

REM CLEAR ALL KILL ALL MOTION REQUEST
REM IN ADDITION, CLEAR ALL STOP MOVE REQUEST
CLR 8467 CLR 522 CLR 523 SET 5647
CLR 8499

REM DISABLE ALL DRIVES
DRIVE OFF X Y
DWL 0.2

REM ISSUE AN ENCODER RES FOR AXIS 0 AND 1
RES X Y
DWL 0.2

REM SET GEAR OFFSET PARAMETER TO ZERO
P12296 = 0
P12552 = 0

REM SETTING THE PPU OF EACH AXIS
PPU X 25000
PPU Y 4000

REM SETTING THE MOTION PROFILE FOR EACH AXIS
ACC 100
DEC 100
VEL 30
STP 100

REM ENABLE DRIVES USED
DRIVE ON X Y

REM SETTING THE GEAR SOURCE AND MODE OF OPERATION
GEAR SRC X RATCH0 Y RATCH1
RATCH0 SRC P6272
REM IN MODE 3, NORMAL FOR POSITIVE PULSES
REM AND BUFFER NEGATIVE PULSES
RATCH0 MODE 3
RATCH1 SRC P6272
RATCH1 MODE 3

REM SETTING THE GEAR PPU OF EACH AXIS
GEAR PPU X4000 Y4000
REM SETTING THE GEAR RATIO OF EACH AXIS
GEAR RATIO X5 Y-2.5
REM ENABLE RATCH FOR AXIS
GEAR ON X Y

ENDP

With the sample code above, the required values for calculating the GEAR OFFSET PARAMETER are

Source count or source value = P6272
GEAR PPU X = 4000, Y = 4000
GEAR RATIO X = 5 , Y = -2.5
PPU AXIS X = 25000, Y = 4000

Sample Calculation for P12296:

With P6272 = 4168
Value1 = 1.042
Value2 = 5.21
GEAR OFFSET PARAMETER = 130250

Sample Calculation for P12552:

With P6272 = 4168
Value1 = 1.042
Value2 = -2.605
GEAR OFFSET PARAMETER = -10420
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.