Home Technologies Electromechanical Group Electromechanical Knowledge Base How fast is my servo axis moving?
Electromechanical Group
  • Technologies
  • More
Electromechanical Group
Electromechanical Knowledge Base How fast is my servo axis moving?
  • Electromechanical Support Forum
  • Electromechanical Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Electromechanical Group requires membership for participation - click to join
  • Electromechanical Knowledge Base & Frequently Asked Questions
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
How fast is my servo axis moving?

Print Friendly and PDF
An Axis Parameter has been added to display the Encoder velocity in 'RPM'. This register will display the encoder RPM updated each Period. If RPM factor > 0 then the algorithm turns on to calculate the RPM. This RPM will be determined by the RPM factor for each axis using the following formula.

RPM Factor = 60 / ((Encoder pulse count per unit) * Servo Period)

Encoder pulse count = (Encoder pulses per revolution * encoder multiplier * encoder revolutions per unit)
{Typically the PPU of the Axis}

AXIS0 AXIS1 AXIS2 AXIS3 AXIS4 AXIS5 AXIS6 AXIS7
RPM Factor P12370 P12626 P12882 P12128 P13394 P13650 P13906 P14162
Actual RPM P12371 P12627 P12883 P12129 P13395 P13651 P13907 P14163
AXIS8 AXIS9 AXIS10 AXIS11 AXIS12 AXIS13 AXIS14 AXIS15
RPM Factor P14418 P14674 P14930 P15186 P15442 P15698 P15954 P16210
Actual RPM P14419 P14675 P14931 P15187 P15443 P15699 P15955 P16211
Usage example:
The motor encoder has a 500 PPR, the ACR card has the multiplier set to MULT 4 and the axis has 2.5 encoder revolutions per inch of travel.

REM Encoder pulse count = (500 * 4 * 2.5) = 5000
REM Default PERIOD = 0.0005
REM RPM Factor = 60 /(5000 *0.0005) = 24
REM P12370 = 24

100 P12370 = 60 /(5000 *0.0005)
120 PRINT "Encoder RPM = ";P12371


Sample program to display average RPM
ATTACH MASTER0
ATTACH SLAVE0 AXIS0 "X"

MULT X4
PPU X5000
ACC 100
DEC 100
STP 100
F 100

REM Set value of RPM factor
P12370 = 60 /(5000 * 0.0005)

10 RES X
REM Set random Feedrate (5-100)
20 LV2 = ((RND 90)+5)
30 F (LV2)
REM Set random distance (5-30)
40 LV3 = ((RND 25)+5)
50 X (LV3)
60 DV0=0 : LV1=1
70 INH 516
80 PRINT" Feedrate = "; LV2;" Distance = ";LV3

REM Add RPM samples to average
200 DV0 = (DV0 + P12371)
REM Count number of samples
220 LV1 = (LV1+1)
REM Loop if axis still moving
240 IF (BIT 516) THEN GOTO 200
260 DWL 0.1
300 PRINT " Number of samples = ";LV1
320 PRINT USING "##.##";" Average RPM = ";(DV0/LV1)
340 PRINT " "
360 DWL 5
380 GOTO 10
400 END


DIM LV5
DIM DV1
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
Ā© Parker Hannifin Corp 2022
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
  • Community Terms of Use
ENGINEERING YOUR SUCCESS.