The quest for compact dust collectors in the industrial manufacturing arena has led to the increased use of filter cartridges. Among these dust collectors is one developed by a manufacturer using PowerCore® filter cartridges. When filtering dust that doesn’t easily release from the filter media, cartridges often plug and restrict airflow. Soon, several customers and operators of these smaller dust collectors found themselves dealing with filter issues and contacted Parker for a solution.
The innovative TotalPleat™ aftermarket replacement filter was developed to fit Donaldson PowerCore® CP filter part numbers P032358-016-340 and P280356-016-340. The proprietary MERV 15 filter provides numerous improvements and advantages over the OEM filter.
Download your copy of the TotalPleat™ Smart Brief Success Story.
The design
Our engineering team used advanced engineering tools, computational fluid dynamic modeling, and 3D printing to design a filter cartridge that can handle more demanding conditions. Innovations like our louvered grid on top of the filter not only more evenly distribute the cleaning air but also serves as a handle for cartridge removal and ASHRAE 199 testing validated the new design.
The installation | case study
After extensive analysis, laboratory, and beta-site testing, some of the first BHA® TotalPleat™ cartridges were installed in September of 2019 in a collector in the southeast United States. The collector, on top of a cement loadout silo, is in plain view of the adjacent interstate and visible dust emissions would attract immediate attention.
With the new TotalPleat™ cartridges, a remote monitoring device was installed to track the collector’s performance. As of December 2020, there had never been any visible emissions from the TotalPleat™ filters and differential pressure has been excellent (see chart on page 2 for the dp trend).
Application detailsThe cement dust filtered by the TotalPleat™ cartridges has more moisture than normal, can be sticky, and harden on the filter media when the moisture condenses. The intermediate use of this collector favors condensation and moist dust. To avoid excessive dust buildup, the cartridges are cleaned continuously during collector operation. Off-time, the time between pulses is 23 seconds and results in one complete cleaning cycle every three minutes. The continuous cleaning requires a tough filter media to withstand the high number of impacts generated by the pulse valves. By December 2020, the cartridges had received over 45,000 pulses, there are no emissions and the differential pressure is still quite low, overall: very good.

Results
A year-plus after installation and without any maintenance, the TotalPleat™ filters are still running strong while the original OEM cartridges had emission and pressure drop problems within the first three months of operation. In several instances, TotalPleat™ life has quadrupled compared to the OEM cartridge, as reported by customers.
What is noteworthy is that during the first days of operation, the TotalPleat™ filters were slightly damaged because the header pressure for the pulse valves was accidentally set to 100 PSIG instead of 60 PSIG. This has not caused any operational issues or emissions and speaks well for the robust new design.
Why do the TotalPleat™ filters perform better?
Pleated filters and cartridges pack a lot of filtration surface into a small space. This results in narrow gas passages that get clogged by sticky dust. Optimizing pleat geometry to balance filtration area, gas velocities, and dust release was key to the advanced performance of the TotalPleat™ cartridge. The louvered grid improved cleaning efficiency by properly distributing the cleaning energy to the entire pleat pack. That is why BHA® TotalPleat™ has longer filter life and the ability to better discharge the accumulated dust. The TotalPleat™ filter cartridges are a direct replacement for the Donaldson PowerCore CP filter part numbers P032358-016-340 (MERV 13) and P280356-016-340 (MERV 15). TotalPleat™ cartridges are completely incinerable.
Download your copy of the TotalPleat™ Smart Brief Success Story.
This blog was contributed the Filtration team, Parker Industrial Gas Filtration and Generation Division.
Powercore® is a registered trademark of Donaldson Company, Inc.
Related content
Defining Our Unique Contribution to the World
Foundry Eliminates Shutdowns and Extends Baghouse Filter Life
Filter Upgrade Improves Bin Vent Dust Collector Performance
Choosing the Best Dust Collector for Air Quality Control in Manufacturing
Reducing Dust Collector Maintenance and Energy Costs in the Cement Industry | Case Study
BHA® Pleated Filter Elements Improve Dust Collection for the Foundry Industry
Choosing the Best Dust Collector for Air Quality Control in Manufacturing

The COVID pandemic impacted the way many industries do business, and the HVAC industry is no exception. Ongoing concerns regarding infection risk and indoor air quality have prompted an unprecedented demand for filters with a Minimum Efficiency Reporting Value (MERV) value of 13, commonly known as MERV 13 filters, as well as those with even higher MERV ratings. As part of its COVID response, ASHRAE recommends increasing outside air within buildings as much as possible, as well as upgrading air filters to a minimum MERV 13 efficiency rating.
Since the introduction of aviation fuel monitor cartridges in aviation fueling, super absorbent polymers (SAP) have been the essential materials used in the final stage of airport ground fueling systems for the protection of on-board systems from water contamination. The material’s ability to absorb and chemically lock in water have its challenges―potential media migration downstream. In 2017,
Two locations were selected and testing was done at these airport tank farms. These tests were accelerated with more than 10 times the typical daily throughput. Upon completion, filters were sent back to our Velcon lab and a witness was present, through EI, to verify the water removal capabilities. Test runs from the two trial locations show vessel throughputs of over 3 million and 5 million gallons per vessel.
There are three available technologies:
Our water barrier filter technology was further developed for general aviation fueling applications.
Parker Velcon has also developed an electronic water sensor for detecting water and fuel. It meets the 1598 design criteria and it was developed to replace chemical water testing. It detects water from zero to 50 parts per million, utilizes a one-quarter-inch common standard port connection, will be certified to ATEX and IECE X, easily to install without any plumbing or electrical systems. And a control box is also available if desired.
Article contributed by Robert Guglielmi, business development manager, 
If you want to find out how you can ASSURE the performance of high efficiency GTs, the answer is multi-faceted. It requires deep understanding of real-world operating conditions and the demands of these impressive machines. And an understanding of what really matters inside the inlet house – and that can only come from experience.
clearcurrent® ASSURE range of filters features an innovative design that helps to boost GT performance, reduce lifecycle costs, improve safety, increase availability and extend GT life. Features and benefits include
This post was contributed by Tim Nicholas, market manager, PowerGen,