Today, the food industry faces demands for all types of produce, from exotic tropical fruits to the staple diet of bread, rice and potatoes, to be available all year round in “just produced” condition. Health concerns over reducing salt, chemicals and preservatives in food places additional pressure on suppliers and manufacturers to find safe, economical ways to extend shelf life. As a result, retailers recognize the need for improvements in packaging technology.
Food products begin to deteriorate almost as soon as they are picked or prepared for packaging. Bacteria, yeast, moisture, and mold are the culprits. The goal of food manufacturers and processors is to delay decay to allow more time from production to the consumer without sacrificing quality.
Modified atmosphere packaging (MAP) is a process that has been used for many years to combat food spoilage. MAP involves packaging or storing product in a modified form of the Earth’s natural atmosphere. Air inside a package is displaced with a protective gas to keep oxygen at controlled levels (less than 2 percent). Too much oxygen and moisture in a package leads to bacterial growth and oxidation, which results in spoilage, inconsistent flavors, poor product quality, and shortened shelf life. Nitrogen gas is usually used as a protective gas in MAP because of its dry, inert qualities.
Typical food products that benefit from MAP- Snack foods such as potato and corn chips
- Nuts
- Meats, poultry, and fish
- Cooked meats, poultry, and fish
- Edible oils
- Coffee and tea
- Powdered milk
- Spices, pasta, and other dried products
- Breads
- Grated cheese and other dairy products
- Salad
- Fruits and vegetables
- Beverages
- Preserving flavor, texture, taste, aroma, and nutritional value
- Increased sales from higher product quality
- Fewer recalls
- Increased production efficiency with longer product runs
- Extended shelf life
- Increased export opportunities to new geographic areas
Nitrogen has traditionally been supplied in the form of high pressure cylinders, liquid mini tanks or bulk storage vessels. However, a delivered nitrogen supply can present a host of problems including:
- Selecting a reliable vendor
- Space allocation for gas storage
- Concerns over purity variations from cylinder to cylinder
- Developing procedures for monitoring and managing the gas supply as well as arranging deliveries and payment plans
- Performing regular leak checks
- Creating a safety plan for storing high pressure gas on-site
- Training workers on how to handle high pressure cylinders and what to do in a crisis situation
Producing nitrogen on-site from compressed air is an economical alternative to buying it. A Parker nitrogen generator, for example, is a plug and play system that uses standard plant compressed air to produce high purity, food grade nitrogen. Installation involves connecting a compressed air line to the inlet and connecting the outlet to the nitrogen line. The system is designed to produce a continuous and consistent supply of commercially sterile nitrogen.
Advantages of a nitrogen generator over a traditional nitrogen supply
- Enhanced safety without the need to store or handle high pressure cylinders
- On demand supply eliminates downtime due to running out of gas or cylinder changes
- Up to 80% cost reduction
- Consistent flow, pressure, and purity
- Compact, space-saving design
- Flexible, modular design
- Low cost of ownership
- Proven reliability
To learn more about in-house nitrogen generation for modified atmosphere packaging, read this brochure. You can also call 1-978-858-0505 to speak with a Parker applications engineer.
This post was contributed by the Gas Generation Technology Blog Team, Parker Hannifin
Related posts:
How to Select an On-Site Nitrogen Generator
Nitrogen: A Cost Effective Way to Extend Food Shelf Life
Optimum Nitrogen Purity for Modified Atmosphere Food Packaging
The Importance of a Food Grade Compliant Nitrogen Gas Supply
Nitrogen generation: an alternative to CO2 in food-grade applications
The COVID pandemic impacted the way many industries do business, and the HVAC industry is no exception. Ongoing concerns regarding infection risk and indoor air quality have prompted an unprecedented demand for filters with a Minimum Efficiency Reporting Value (MERV) value of 13, commonly known as MERV 13 filters, as well as those with even higher MERV ratings. As part of its COVID response, ASHRAE recommends increasing outside air within buildings as much as possible, as well as upgrading air filters to a minimum MERV 13 efficiency rating.
Since the introduction of aviation fuel monitor cartridges in aviation fueling, super absorbent polymers (SAP) have been the essential materials used in the final stage of airport ground fueling systems for the protection of on-board systems from water contamination. The material’s ability to absorb and chemically lock in water have its challengesāpotential media migration downstream. In 2017,
Two locations were selected and testing was done at these airport tank farms. These tests were accelerated with more than 10 times the typical daily throughput. Upon completion, filters were sent back to our Velcon lab and a witness was present, through EI, to verify the water removal capabilities. Test runs from the two trial locations show vessel throughputs of over 3 million and 5 million gallons per vessel.
There are three available technologies:
Our water barrier filter technology was further developed for general aviation fueling applications.
Parker Velcon has also developed an electronic water sensor for detecting water and fuel. It meets the 1598 design criteria and it was developed to replace chemical water testing. It detects water from zero to 50 parts per million, utilizes a one-quarter-inch common standard port connection, will be certified to ATEX and IECE X, easily to install without any plumbing or electrical systems. And a control box is also available if desired.
Article contributed by Robert Guglielmi, business development manager, 
If you want to find out how you can ASSURE the performance of high efficiency GTs, the answer is multi-faceted. It requires deep understanding of real-world operating conditions and the demands of these impressive machines. And an understanding of what really matters inside the inlet house – and that can only come from experience.
clearcurrent® ASSURE range of filters features an innovative design that helps to boost GT performance, reduce lifecycle costs, improve safety, increase availability and extend GT life. Features and benefits include
Download our white paper, "Driving Gas Turbine Efficiency: Maintaining Greater than 60% Efficiency for Gas Turbine in Power Generation" to learn more
This post was contributed by Tim Nicholas, market manager, PowerGen,