Shoppers’ expectations for high quality, healthy and conveniently accessible food products result in an ever-increasing demand on producers and packers. In Europe, suppliers must adhere to a series of strict legislative measures in order to deliver food that is safe to consume. The challenge many suppliers face is that the food they supply must satisfy the consumers’ needs of freshness and value for money.
With growing public knowledge of the issues surrounding the use of chemicals and preservatives in food production, suppliers must seek alternative methods for food preservation.
Spoilage begins instantly
As soon as a crop is harvested or an animal is slaughtered, the yield must be preserved. Nitrogen is commonly used to inhibit spoilage mechanisms in all stages of processing.
According to the European Union directive 2009/10/EC, when nitrogen is used as a preservative, it is classed as a food additive and is designated an ‘E’ number — E941. This means it must comply with food additive regulation 1333/2008.
The European specification for food grade nitrogen gas defines a maximum remaining oxygen content of less than 1%, (99% nitrogen). The specification for food grade nitrogen gas is determined by the European Industrial Gases Association, (EIGA), in conjunction with the Joint Expert Committee on Food Additives, (JECFA), and can be found in their publication IGC Doc 126/11/E.
For more details, please download our white paper, Parker Nitrogen Gas Generation for Modified Atmosphere Packaging, (MAP).
Methods of supply
In order to observe the terms within the legislation, care must also be given to the suitability of the materials of construction in which the method of supply occurs.
The International Organisation for Standards (ISO) outline in ISO/TS 220022-1:2009 measures related to the construction of equipment designed to produce and convey nitrogen gas to food applications including processing, blanketing or modified atmosphere packaging. It states:
“Compressed air, carbon dioxide, nitrogen and other gas systems used in manufacturing and/or filling shall be constructed and maintained so as to prevent contamination.”
“Gases intended for direct or incidental product contact (including those used for transporting, blowing or drying materials, products or equipment) shall be from a source approved for food contact use, filtered to remove dust, oil and water.”
A compliant nitrogen supply
In both engineering development, and technical support, Parker employs dedicated, expert resources to ensure all equipment is designed, manufactured and supplied to meet the ever-demanding applications within the food processing sector. By understanding the detailed compliances needed to meet EU legalization, Parker is able to support its customers and ensure they have the correct equipment in place.
Both the Parker NITROSource and NITROSource Compact nitrogen generators produce fully compliant, food grade nitrogen. All of the components that contact the generated nitrogen gas stream are compared or analyzed to reference standards for materials of construction covering food use, under the most stringent of global standards — the United States of America Food and Drug Administration (FDA), Article 21.
Parker prides itself in guaranteeing that if the equipment, including air treatment and nitrogen generators, are installed and maintained correctly, the producer will deliver both compressed air and nitrogen gas in line with EU regulations to their application. This is further backed by third party validation from both Lloyd’s Register and Edward’s Analytical.
For additional information on Parker NITROSource and NITROSource Compact nitrogen generators, please visit our website or download the NITROSource Compact product brochure.
The aim of MAP is to prevent or slow down food spoilage mechanisms that alter the appearance, smell, taste, shelf life and safety of the product. Please download our white paper, Parker Nitrogen Gas Generation for Modified Atmosphere Packaging, (MAP), to learn more about the solutions that Parker offers.
This post was contributed by Phil Green, industrial gas application manager, Parker Gas Separation and Filtration Division EMEA.
Related posts
Nitrogen: A Cost Effective Way to Extend Food Shelf Life
Modified Atmosphere Packaging with a Nitrogen Generator
How to Select an On-Site Nitrogen Generator
Top Frequently Asked Questions About Nitrogen Generators
The COVID pandemic impacted the way many industries do business, and the HVAC industry is no exception. Ongoing concerns regarding infection risk and indoor air quality have prompted an unprecedented demand for filters with a Minimum Efficiency Reporting Value (MERV) value of 13, commonly known as MERV 13 filters, as well as those with even higher MERV ratings. As part of its COVID response, ASHRAE recommends increasing outside air within buildings as much as possible, as well as upgrading air filters to a minimum MERV 13 efficiency rating.
Since the introduction of aviation fuel monitor cartridges in aviation fueling, super absorbent polymers (SAP) have been the essential materials used in the final stage of airport ground fueling systems for the protection of on-board systems from water contamination. The material’s ability to absorb and chemically lock in water have its challenges―potential media migration downstream. In 2017,
Two locations were selected and testing was done at these airport tank farms. These tests were accelerated with more than 10 times the typical daily throughput. Upon completion, filters were sent back to our Velcon lab and a witness was present, through EI, to verify the water removal capabilities. Test runs from the two trial locations show vessel throughputs of over 3 million and 5 million gallons per vessel.
There are three available technologies:
Our water barrier filter technology was further developed for general aviation fueling applications.
Parker Velcon has also developed an electronic water sensor for detecting water and fuel. It meets the 1598 design criteria and it was developed to replace chemical water testing. It detects water from zero to 50 parts per million, utilizes a one-quarter-inch common standard port connection, will be certified to ATEX and IECE X, easily to install without any plumbing or electrical systems. And a control box is also available if desired.
Article contributed by Robert Guglielmi, business development manager, 
If you want to find out how you can ASSURE the performance of high efficiency GTs, the answer is multi-faceted. It requires deep understanding of real-world operating conditions and the demands of these impressive machines. And an understanding of what really matters inside the inlet house – and that can only come from experience.
clearcurrent® ASSURE range of filters features an innovative design that helps to boost GT performance, reduce lifecycle costs, improve safety, increase availability and extend GT life. Features and benefits include
Download our white paper, "Driving Gas Turbine Efficiency: Maintaining Greater than 60% Efficiency for Gas Turbine in Power Generation" to learn more
This post was contributed by Tim Nicholas, market manager, PowerGen,