Innovations in rail travel are making trains faster, safer, more efficient and environmentally friendly. Of all the transportation modes, rail is leading the way in new technologies.
Electric railways are becoming more common in response to both environmental and cost concerns. High-speed rail technology is promising speeds beyond 300 mph in a matter of a few years. And, without a doubt, rail transport is more autonomous than other forms of transportation.
Let’s start by taking a look at what is happening with regard to railway electrification.
Most high-speed trains today get their electricity from overhead wires or catenaries using a pantograph. That’s because, given current designs and technologies, batteries can’t be sized to supply the necessary power and still fit on the train. Diesel engines turning generators don’t meet new environmental mandates. Plus, the weight, storage demands and costs of diesel fuel, along with fire safety concerns, create added challenges. Another option has been to use a shoe to take electricity from a third rail (similar to light rail), but this has proven to create too much friction between the shoe and rail at high speeds.
A major challenge when using pantographs to take power from the catenary is maintaining consistent contact between the two without creating too much friction. Most pantograph systems work on compressed air. An auxiliary compressor can deliver the needed air supply, but this method has proven costly and the compressor takes up valuable space that could be put to better use in optimizing capacity for freight or passengers.
Several companies have invested in alternatives. Parker eliminated the need for an auxiliary compressor by designing a compact, fully integrated “plug and play” control system, which contains all the pneumatic functions along with a reservoir. The redesigned main control module system is linked to the reservoir, from which the pantograph system draws compressed air. This solution is attractive since it’s lightweight, space-efficient, less expensive and requires fewer components that need to be maintained and replaced.
Another issue that crops up with catenaries is ice on the overhead wires. To combat this problem, some trains are deploying two pantographs so that the first one knocks off the ice. To handle travel in either direction, train makers often package a pair of pantographs in the same overhead fairing, mounting them face-to-face.
Along with the desire to convert more diesel locomotives to electricity is an interest in minimizing or reusing electric energy. Beyond the obvious environmental benefits are cost advantages, since energy (fuel) represents the largest cost component in total transport costs. This has led to an increased interest in many energy-saving technologies like regenerative braking that converts the kinetic energy from the braking motion into electric energy for purposes of energy reuse. Electricity is then fed back through the overhead lines so it can power an accelerating train on another track or be stored for future use.
Challenges remain, however, to find sufficient space for storing electricity. When there is no place to store or use the electricity, it gets burned off in roof-mounted braking resistors (rheostatic braking) or the train switches to friction braking.
Energy storage systems are currently available in multiple forms. Some of the more common include flywheels, electric double-layer capacitors, batteries, fuel cells and superconducting magnetic energy storage devices. In evaluating the various options, attention is paid to their high energy density and power density, as well as their total cost, environmental impact, space efficiency and weight.
In general, battery-based energy storage systems have higher energy densities but their capital costs are often higher, and they have more limited lifespans. The market is looking for technology breakthroughs that will lower the cost of the storage systems. By 2030, for example, it is expected that the cost of lithium-ion batteries will drop considerably due to technology advances regarding their design and production. There are, however, environmental drawbacks of batteries since they use toxic materials. Flywheels offer the greatest environmental appeal, but the future ideal solution is seen as one that will combine the advantages of different energy-storage technologies.
Regenerative braking is preferred because, in addition to its obvious energy efficiency, it minimizes wear and tear. Another option, however, is the use of linear eddy-current brakes which consist of electrical coils positioned along the rails. The coils serve as magnets with continually switched north and south poles. When the magnets move along the rail, their changing magnetic field creates another field in the metal rail, which creates electrical tension and eddy currents to provide enough resistance to slow the train.
Improving train aerodynamics is yet another way to significantly affect energy usage, since up to 60% of the tractive force can be lost due to drag and friction. Covering roof-mounted equipment with streamlined fairings also reduces drag and limits the booming sound trains make when traveling through a tunnel.
Solar rail is a relatively new concept for producing clean energy for railways.
Australia has been effectively using solar panels on the roofs of its electric rail cars since 2017.
Hydrogen power is also being explored for greater sustainability. With this technology, fuel cells would consist of an anode, cathode and electrolyte membrane. Hydrogen would pass through the anode where it splits into electrons and protons. As the electrons are pushed through a circuit, they would generate an electric charge that is stored in lithium batteries or directly used by a train’s electric motor.
As is the case with some other technologies designed to conserve energy, the hydrogen concept needs to be perfected to ensure cost competitiveness and safety.
Research is ongoing to make trains even faster and more energy efficient in the future.
In the area of high-speed rail technology, superfast maglev trains are gaining momentum. Key to their ability to reach unmatched record speeds is the use of magnets that float carriages above the ground without wheels. The technology already is being used in Europe with a second-generation technology being promised to hit the market by 2027 offering speeds in the 300+ mph range.
Elon Musk is additionally touting a hyperloop that would hit speeds up to 700 mph. The hyperloop consists of a vacuum-sealed tube that reduces air resistance and carries “pods” using passive maglev technology.
These examples represent just a few of the many innovations being explored to accelerate the speed and energy efficiency of today’s railways.
With the higher speeds, however, come greater concerns regarding safety and the added burden on various components, including increased vibration and heat.
Fire safety was a focus of Europe’s EN 45545 initiative which outlined new safety requirements for railways, especially regarding fire concerns. Parker was the first hose manufacturer in Europe to develop rail hoses using a new rubber compound that meets the requirements of EN 45545, while also offering cost savings and easy installation with its improved bend radius.
This article contributed to by Dave Walker, market development manager, Rail, Motion Systems Group, Parker Hannifin.
Related content
Defining Our Unique Contribution to the World
Improving Efficiency of Marine Desalination Systems
Clean Transportation: Hybridization and Electrification in the Marine Industry
Rail Overview: On the Right Track for Tomorrow
Parker Solutions for the Transportation Industry
What Every Design Engineer of Rail Vehicles Should Know About EN 45545
Pneumatics Technology Enhances Profitability in Rail Applications
Looking ahead to the future of industry, with all the advancements in technology that the Industrial Internet of Things (IIoT) holds in store, one might rightly wonder if pneumatics will still have pride of place on the production line. After all, it’s basically just gas or air passing through tubes! Surely all the innovation that’s happening with digitalisation will mean that IIoT components will become much more important than the pneumatics?
Pneumatics and IIoT inseparable
In actual fact, the real answer is that the two technologies will most likely become inseparable because they perform equally important functions that are increasingly becoming interdependent. Parker’s recent ‘Factory of the Future’ market research has revealed that pneumatic technology will indeed remain a critical component in the digital manufacturing field for the foreseeable future. Although pneumatic equipment indeed functions through pressurised gas or air moving through tubes, these tubes remain the ‘veins’ of the factory, delivering fast, precise and efficient movement on complex automation lines and facilitating quick and easy assembly, cleaning and a host of other functions on the production floor.
Pneumatic designs compliment approach of Industry 4.0
Since pneumatics have been around for quite some time, they already offer high reliability and efficiency, and their designs naturally complement the modular approach of Industry 4.0. In the increasingly digital manufacturing sphere, pneumatic systems are being adapted to answer the need for real-time process data through the incorporation of IIoT enabled nodes and sensors.
Although some pneumatics manufacturers have been slow off the mark to follow the digitalisation trend, Parker recognised the opportunity to serve customers with industry-leading connectivity and safety solutions well in advance. For instance, our entire product development cycle is now focused on making devices ‘smart’ by ensuring that they are able to communicate their status to the rest of the network. OEMs can now easily use these smart pneumatics equipped with cost-efficient sensors to intelligently monitor the real-time status, positioning, velocity, condition and efficiency of the various components that make up the modern automation line.
Although there is still a long road to travel in order to realise the ultimate vision of Industry 4.0, the intermediate period will see the gradual introduction of these smart products that offer both traditional control functions and actionable intelligence. The evolution of manufacturing is contingent upon the development and continuous improvement of this actionable intelligence, giving users the ability to track the uptime and availability of the machines in their plant. The analytics from this data will enable significant operational cost savings, for instance by performing predictive maintenance and achieving optimised operations using continuous position sensing.
Choices ahead to future-proof designs
While the technology is still in a state of flux, machine builders and their component suppliers will now need to make careful choices in order to future-proof their designs. Parker believes that open-source, low-cost Industrial Ethernet (IE)-based components and subsystems is the answer to this challenge, and so our recent product development efforts have been based on IO-Link enabled connectivity and network solutions.
IO-Link enabled products are just one example of how Parker, leading with purpose, is providing customers with cutting edge technologies for use in globalised manufacturing operations. Regardless of location, the use of IE and IO-Link network nodes make the control, safety and maintenance of a range of different devices, machines, systems and users simple and cost-effective.
Ensuring that key automation components such as pneumatic valves are IIoT-enabled is an excellent way of creating white space opportunities for innovation in the factory of the future.
Learn more
To discover more about Parker’s I/O Link IIoT solution, please download our brochure IO-Link Solutions here.
Article contributed by Richard McDonnell, marketing development manager (IoT & Smart Products) Pneumatic Division, Parker Hannifin Corporation.
What is the Foundation for a Smart Factory?
Industry 4.0 is Taking Place in Front of Our Eyes
The Importance of Reliable Connectivity Between Industrial Ethernet and Pneumatic Valves
Parker Teams Deploying IoT to Help Customers Improve Operations
Linear actuators are used in many applications around industry. Pneumatic, hydraulic and electromechanical technologies are the primary options for providing linear actuation but the selection and use of these technologies depends greatly on technical knowledge, budgets, available energy sources and careful consideration of the performance trade-offs of different approaches.
For example, pneumatic actuators don’t deliver high force output but are practical when a cost-effective, easy start-up is required. Conversely, hydraulic linear actuators are suited to high force applications but generate a lot of noise. And, while electromechanical actuators are quieter, they are much more difficult to install and maintain.
So, what are the considerations and trade-offs when selecting linear actuators for a linear motion application?
Pneumatics
There have been several recent improvements in pneumatic design, including positional feedback capabilities from proximity and linear position sensors. Better sealing has also allowed pneumatic linear actuators to be used more often in challenging environments or applications requiring wash down.
However, pressure losses and the compressibility of air can make pneumatics less efficient than other linear technologies. While the speed ranges from a couple of centimetres per second to 150cm/s, force output is dependent on the maximum pressure rating and related bore size. Typically, however, pneumatic actuators have a maximum pressure rating of 10bar with bore sizes ranging from 12 to 320mm for approximately 80N to 80kN.
Hydraulic systems therefore have a much higher possible force output, with typical pressure ratings up to 210bar with bore sizes ranging from approximately 12 to 355mm translating to about 220 to 171,000N of force. Hydraulic actuation also generates a significant amount of noise and, without proper maintenance, can leak.
Electromechanical
When driven by a rotary motor, electromechanical linear motion systems employ one of four rotary-to-linear conversion systems: ballscrew, roller screw, Acme (lead) screw or belt drive. In addition, a linear motor can be used to provide motion.
A linear motor is similar to a rotary motor, but the motor coils make up the forcer. Depending on the design, one or two rows of magnets comprise the magnet track. In a rotary motor, the rotor spins while the stator is fixed, but in a linear motor, either the forcer or the magnet track can be the moving component, which is then integrated with an appropriate linear bearing. By sending electrical current to the forcer, the resulting magnetic field interacts with the magnet track and drives the linear motor carriage back and forth.
Linear motors have high dynamic performance, with acceleration of greater than 20G at velocities of 10m/s or higher. Due to the direct drive nature of linear motors, there are no mechanical components to add backlash, torsional wind-up, or other positioning errors. Sub-micron resolution and repeatability are achievable and as the motor is directly coupled to the load, there are fewer components to fail, which adds long-term reliability.
Making a measured choice
Pneumatic, hydraulic and electric actuators are an integral part of automated systems, and there is no better actuator than another as the choice depends on the peculiarities and application needs. Today, the three technologies appear to be well developed and with a good level of maturity that guarantees long life and good reliability although with different operating characteristics. Placing a priority on one type of application parameter could mean that performance in another area might be sacrificed, but nevertheless all the decision making categories should be carefully weighed up before making the final choice of actuator equipment.
This article was contributed by Franck Roussilon, product manager, Pneumatic Division Europe, Parker Hannifin Corporation.
How to Install Pneumatic Cylinders to Maximise Life and Performance
High-load Rodless Actuators Powering the Factory Automation Revolution
Challenged with Long-Stroke Hydraulic Cylinder Performance? Read This
.
IO-Link is a point-to-point communication technology that can be implemented into most PLC configurations or integrated into most existing industrial Ethernet networks via a device called IO-Link master. It is the first standardized IO technology worldwide (IEC 61131-9) for point-to-point communication between sensors, actuators and control devices – comparable to an “industrial USB” and is the perfect local extension of a superior industrial Ethernet network. Thanks to its simple installation, better control and enhanced diagnostics capabilities, IO-Link has already secured a large user base.
There are multiple advantages for engineers when designing an IO-link architecture for their latest equipment. For example: when applying a Parker IO-Link connected Moduflex valve island, in addition to simplified and standardized wiring, they can also realize the benefits of remote configuration, monitoring, and increased data availability, leading to enhanced diagnostics. Utilizing IO-Link can also be especially beneficial for machine applications where there are frequent changeovers or reconfiguration as this time can be reduced, as can unplanned downtime.
How to install IO-Link
IO-Link doesn’t require any special or complicated wiring, which is a major benefit for adopting it as a communication method. Instead, IO-Link devices can be connected using standard 3 or 5-wire M12 cables, the same you would use to connect a standard proximity switch.
If previously you were using 25-pin wiring for a pneumatic valve manifold, then an upgrade to IO-Link would offer similar diagnostics and performance as with an industrial network (e.g. Profinet) but at a significantly lower cost and with a less complex system:
• Highly cost-effective solution - It replaces an analog I/O and its 4-20mA/0-10V signal with the IO-Link digital information from an analog sensor, or to an analog device such as pressure regulator, saving on inventory costs
• Enables possibilities for customer to de-centralize devices - On small- to medium-sized machines, many of the available IO-Link masters are IP67 and can be placed on the machine near the I/O points instead of in a centralized cabinet
• Suitable for SAFE power source - Some IO-Link devices, such as the Parker’s IO-Link valve islands solution, are even suitable for use with a SAFE power source which is becoming an important requirement on many markets due to machine directives
Data availability and maintenance
IO-Link offers an increase in availability of data to the PLC, which helps to reduce time and money spent on troubleshooting analysis. There are three data types available:
• Process data – Cyclic information that is transferred between device and the master automatically on a regular basis, used as I/O for the machine controls
• Service data – information about the device itself, such as model and serial number, or error messages and maintenance warnings (e.g. device overheating, maximal current is exceeded, coil short circuit)
• Parameter data – information that can be written in, or read from the device on request such as voltage level or counting cycles to support preventive maintenance needs
With IO-Link, you can read and change device parameters through the control system software which enables faster configuration and commissioning, plus changes can be made dynamically from the control system as needed. IO-Link also offers the ability to monitor device outputs, receive real-time status alerts, and adjust settings from virtually anywhere. Users can identify and resolve problems that arise in a timely manner and make decisions based on real-time data from the machine components themselves.
With visibility into errors and health status from each device, users can see not only what the device is doing but also how well it is performing. These extended diagnostics allow users to easily identify when a device is malfunctioning and diagnose the problem without shutting down the line or machine. The combination of real-time and historical data available via IO-Link helps to ensure smooth operation of system components, simplifies device replacement and enables the operator to optimize machine maintenance schedules – saving cost and reducing the risk of machine downtime.
Many general pneumatic control applications can benefit from such modules, including packaging machines, automotive systems and factory automation. In fact, if you happen to visit any automotive or packaging facility, the ‘elephant in the room’ will be clear to see: the big controller cabinet housing the PLCs and contactors. These cabinets consume valuable floor space, but now they are set to shrink in size. Safety relays are increasingly moving out of the cabinet, and trends indicate that PLCs are soon to follow. This ‘do more with less’ business model should encourage any of you who typically still hard-wire valve manifolds, to make that leap towards industrial networks such as IO-Link.
Use our configurator on Parker.com to discover how you can utilize IO-Link for your application.
Article contributed by Patrick Berdal, EMEA product manager for control devices, Pneumatic Division Europe, Parker Hannifin Corporation.
Related content
Optimise your Connection of Pneumatic Manifolds to Industrial Networks
What is the Foundation for a Smart Factory?
Know Your Pneumatics: Continuous Position Sensing
How to Use Smart Sensors to Aid Predictive Maintenance Strategies
Parker's Central Tire Inflation System (CTIS) offers improved mobility when operating vehicles in severe off-road or soft soil conditions. Ideally suited for the agriculture and military markets, this automatic tire pressure adjustment system allows the driver to optimize tire inflation pressure from the cab while operating on varying terrains with the simple push of a button. Reducing tire pressure results in a bigger tire footprint, providing increased flotation and traction when operating in soft soil terrain. Although often used in conjunction with all-wheel drive, non-all-wheel drive vehicles with CTIS can actually outperform all-wheel drive in many soft soil conditions.
Operating vehicles with reduced tire inflation pressure is approved by tire manufacturers when operating at reduced vehicle speeds. Contrary to common perception, operating at reduced tire inflation pressure can extend tire life due to reduced susceptibility to tire punctures and tread chunking. CTIS also results in increased fuel economy due to the improved rolling resistance as the tire floats on the surface rather than creating ruts in soft soil or sand.
What's included in Parker's CTIS?Each wheel end is equipped with a CTIS wheel valve. The wheel valve connects the tire to the CTIS control system whenever it is actively measuring or changing tire pressure. Otherwise, the wheel valve is closed, isolating the tire from the system, thus ensuring that the tire will not leak down. This eliminates the need for manually operated shut off valves when the vehicle is inactive for extended periods of time. This feature also provides extended air seal life when the vehicle is in motion and tire pressure adjustment is not occurring. Parker offers wheel valves in a variety of sizes and configurations including valves with hose connections as well as flush-mount hose-less versions for use with wheels that have integral air passages. Located on the vehicle chassis or undercarriage, Parker’s CTIS pneumatic control unit consists of electro-pneumatic valves and pressure sensors required to monitor and control the pneumatic system.
CTIS provides independent wheel-end control ensuring fail-safe operation in the event of damage to the vehicle or wheel end. The CTIS wheel valve is completely sealed to the atmosphere at the wheel end ensuring reliable deepwater forwarding capability. Tire venting while deflating is routed back through the pneumatic control unit rather than at the wheel end. The CTIS electronic control unit provides decision making and logic execution. The electronic circuitry is completely sealed in an aluminum enclosure resulting in a rugged environmentally robust package.
How does the CTIS work in certain operating conditions such as extremely soft soil for vehicle mobility?Vehicle mobility is improved by reducing tire inflation pressure resulting in a larger tire footprint. This bigger footprint improves traction, reduces wheel slip and allows the vehicle to float across the soft terrain instead of compacting the soil and causing rutting. When returning to improved terrain conditions, a simple push of a button on the driver interface automatically inflates the tires to the appropriate pressure utilizing the onboard air compressor.
Its unique wheel valve design provides the best in class deflate performance while incorporating the non piloted remote venting control strategy preferred by most vehicle manufacturers. CTIS can deflate tire pressures significantly lower than the competition while operating reliably over a wide range of temperatures and altitudes. The CTIS is insensitive to vehicle installation variables such as wheel-end, the back pressure and air seal flow. This results in enhanced fault tolerance as wheel valve shutoff is assured even with kinked, contaminated or restricted airlines. This is a patented wheel valve design that gets the job done faster, resulting in industry precedent-setting deflation rates. The operator interface provides the ability to select four terrain modes:
Pressing any of the terrain buttons results in the system checking all tire pressures and then automatically adjusting them to pressure targets. A green light on the driver interface will flash while pressure changes are being made and then turn solid indicating that target tire pressures have been reached. The operator can also select from three load levels: no load, partial load and full load optimizing tire pressure for load improves fuel economy, vehicle stability and ride comfort.
The CTIS monitors tire pressure at regular intervals and offers a run-flat mode which reduces this interval to almost continuously monitor pressure. This is useful when an increased threat for puncture exists. CTIS will return to normal pressure check intervals after a predetermined time has expired.
The system also monitors vehicle speed and provides both an over-speed warning and an automatic terrain mode bumper to ensure safe operation operators can run in an overspeed condition for a short period of time, for example, to preselect for an impending terrain change continue to over-speed will result in the amber warning led on the selected terrain button beginning to flash. If the vehicle speed is not reduced within an additional time, CTIS will automatically bump up the terrain mode to a more appropriate setting and inflate the tires to the new target pressure. This staged approach allows the operator to pre-select terrains as needed while protecting tires from damage.
Watch the video to learn more and see a vehicle in action:
Are you headed to IFPE 2020 in March?
Parker off-highway and mobile solutions will be showcased at IFPE/CONEXPO-Con/AGG in Las Vegas March 10 – 14. The Parker CTIS system will be on display. The CTIS offers best in class performance, including tire pressure control range and deflate rates with robust full tolerance. Parker is the global leader in motion and control technologies. For more information regarding Parker's central tire inflation systems, contact us.
Article contributed by Ryan Mills, project engineer, Parker Hannifin's Pneumatics Division.
Related blogs to learn more about pneumatic technology:
How Can Pneumatic Technology Help Farmers Boost Their Crop Yields? Part 1 of 2
Load Sensing Valve Improves Heavy Duty Machine Productivity and Fuel Savings
Split Pump IFC on a Wheel Loader: Simply Smarter
Starting from agriculture and food processing arriving to the packaging operation, automation is everywhere in the modern food plants and plays a fundamental role to address the required control movement quality, production speed, labour savings and overall profitability. Especially for food zones and wash areas, where there are multiple national and international standards to take into account and frequent cleaning and sanitising cycles to support, pneumatics offers a cost-effective choice. Applications in food production typically require specific certification for air motors, pneumatic cylinders and other associated equipment and special clean design features that minimize entrapment points for bacteria.
Environmental challenges
Food production environments necessitate frequent wash-downs of the work area, which can lead to damage to static and dynamic gaskets and seals. Constant exposure to damp and the caustic sprays of hydrogen peroxide and other cleaning materials used in wash-down cycles can eat away at unprotected materials. These environmental challenges have made stainless steel the most commonly used material for all food processing applications. Although stainless steel is more expensive than aluminum, it can resist the steam, high pressure water and caustic cleaners often used in food and beverage production. Parker P1VAS air motor and planetary reduction gear for example is built into a polished stainless housing that is sealed by a fluorocarbon rubber O-ring. The output shaft, which is made of polished stainless steel, is also sealed by a fluorocarbon rubber seal and thanks to the cylindrical shape, there are no pockets that can accumulate dirt or bacteria.
No matter which component is being specified, it’s critical to understand the details of the food processing application and what is required - such as pressure, temperature, flow, port sizes, configurations and locations. Too often, filters or valves are chosen based on cost or size alone, forcing maintenance personnel to spend extra time on maintenance as a result of the system designer’s less than optimal choice. Longevity and repeatability are basic requirements for any good pneumatic solution. The choice should be made on products that have been thoroughly tested and designed to withstand the toughest conditions for operation, vibration and impact.
The accessories and options for pneumatic components are frequently neglected, so it’s important to ensure the entire product can withstand the environment where it will operate to avoid forcing maintenance personnel to waste time replacing parts. For example, the adjustment knob or T-handle of a typical regulator is made of a composite material. The caustic chemicals used in wash-down can corrode many types of plastic, so in addition to a stainless steel regulator, the knob should be made of stainless steel or other compatible material.
Filter-regulator options such as tapped manual drains or automatic stainless-steel drains are widely used to get rid of excess liquid and prevent water from draining onto the floor. Look for non-relieving regulators that do not release gases or liquid into the atmosphere. Whenever possible, select pre-lubricated or lubrication-free mechanisms that use food-grade grease and don’t require periodic lubrication.
Although some pneumatic valves meet NEMA protection standards or IEC/IP ratings, most are designed to be mounted in an enclosure to protect them during wash-downs. Check the design of this enclosure for any crevices between the valves and subplate or manifold bases and other non-smooth surfaces that can harbor bacteria. For those who use serial communications with their valves, these electronics also require protection.
Components that require lubricated compressed air or periodic manual lubrication should be avoided when working in food processing to minimize the risk of product contamination. Lubricant in the compressed air can collect near exhaust ports, and manually applied lubricant can spill onto or collect on multiple components.
Using dry air in non-lubricated applications is critical; condensation can corrode system components, increasing maintenance costs and reducing system efficiency. Also, unless distribution air lines are made of stainless steel, aluminum, or high-strength plastic, water can create pipe scale that can work its way into components and cause malfunctions. Water is a poor lubricant; when emulsified with residual compressor oils, it becomes a milky substance that must be drained away. In addition, there should never be any contact with synthetic emulsions in food processing. Dry, filtered, non-lubricated air usually eliminates these issues.
Learn more
Find out more information about P1VAS air motors in this video.
This article was contributed by Franck Roussilon, product manager, Pneumatic Division Europe, Parker Hannifin Corporation.
Related content
Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments
Know Your Pneumatics: Hints & Tips For Specifying Linear Actuators
All You Need to Know About Air Motor Selection
In the world of industrial automation, pneumatic rodless cylinders can now be found just about anywhere; from food and beverage packaging to pharmaceutical and chemical production lines. They have a significant advantage over more conventional rod-type cylinders because they are fast, efficient, capable of supporting high direct and cantilever loads and are smooth-running. In addition, they require only about half the space compared to their traditional counterparts.
They are also easily adjustable and offer air cushioning at the end positions. This serves to dampen the piston as it reaches the end of its travel, thereby slowing down the speed of the load at the end of the stroke to prevent unnecessary impact or shocks. Without the right setting, the service life of the overall system will be considerably shorter and generate potentially problematic vibrations throughout the entire assembly line.
Adjustable cushioning can be tailored to specific applications and is therefore more efficient than cushioning preset by the manufacturer, which can only assume a standard load and the speed at which it needs to travel. By adjusting the cushioning settings, which is known as “ideal cushioning”, the piston is decelerated to zero velocity at the end of the stroke, thereby dissipating all kinetic energy in the load. Therefore, shorter cycle times are achieved because with no piston bounce, no time is lost due to shock or vibration. System wear is reduced as the ideal cushioning eliminates shocks to the cushioning sleeve, thereby increasing the lifetime of the cylinder. Productivity is also ultimately improved when the system is at optimal operation, working well on a continuous basis without force, shocks or vibrations.
Adjusting the end position cushioningLet us take a look at the correct way to adjust the end position cushioning on a Parker ORIGA OSP-P pneumatic rodless cylinder to ensure shorter cycle time, less wear, higher productivity and longer product lifetime. This is recommended for any Parker rodless pneumatic cylinder before first use.
It is recommended that six bar of operating pressure is used for the adjustment process; any variations in pressure will require a slightly modified adjustment process.
The adjustment screw is located at the cylinder's end caps.
All you will need to perform the adjustment is a small slotted screwdriver.
With the fine thread of the cushioning screw, there is a high degree of sensitivity and set-up can be completed very accurately. The cushioning screw itself is secured against completely unscrewing. The factory setting of a Parker rodless cylinder cushioning adjustment screw is approximately one half turn open.
Firstly, loosen the cushioning adjustment screw by one full turn.
The piston re-bounces from the air cushion causing it to vibrate.
Cushioning must be slowly adjusted by loosening the screw turn-by-turn.
Cylinder noise will increase slightly but the piston vibrations will immediately start to decrease.
The vibrations will continue to decrease as you loosen the cushioning screw.
The noise will continue getting louder - this is completely normal for the adjustment process.
Continue to slowly loosen the cushioning screw until the vibrations stop.
The cylinder will now become quieter until the noise is barely perceptible.
The piston will gently move into the end position.
The adjustment process is complete.
The ideal cushioning will increase productivity and output and will reduce costs at the same time.
Learn moreTo find more information on how to adjust the end position cushioning of the Parker ORIGA Series of pneumatic rodless cylinders, please see this video:
Article contributed by Dieter Winger, Product Manager, Pneumatic Rodless Actuators, Pneumatic Division Europe, Parker Hannifin Corporation
Related content
Know Your Pneumatics: Basics of Rodless Cylinders
3 Ways to Magnify Return on Investment (ROI) on Pneumatic Cylinders
Know Your Pneumatics: Continuous Position Sensing
Test What You Know About Pneumatics
As an engineer, the responsibility to adopt not just the latest, but the safest technologies, never goes away. Protecting people and machinery has become, quite simply, industry’s number one priority. Safety first. Always.
Factory automation is certainly no exception. Here, major advances have fuelled greater focus on smarter controls and increased integration of smart devices and safety componentry. Included in this are the latest pneumatic solutions, which nowadays form a core part of safety controls for implementing the preventative technical measures needed to ensure machine safety, including clamping, blocking, exhausting and holding equipment in place.
But hold on a moment, what actually classifies a product as a safety component? Well, as with all things related to machine safety, the best place to find out is the Machinery Directive, which states that a product is deemed to be a safety component when it is tested and verified to provide specific safe function for a pre-determined period of time in a given state.
The Machinery Directive also offers clear distinction between safety devices and standard pneumatic components deployed in a safety circuit. Notably, the term ‘safety component’ does not imply the actual reliability or safety level of the component. Those products offered as safety-rated must undergo stringent requirements for certification, testing and approval. As a further point, the Machinery Directive does not prescribe the use of safety-rated componentry, it merely provides a description of the conformity assessment procedures to market a product as safety rated.
So, how is it best to determine what level of safety is required? The answer: perform a risk assessment. Three steps are involved here: analysis, evaluation and reduction. The first step, risk analysis, also requires engineers to estimate risk and determine the performance level required (PLr).
After the PLr is established the performance level (PL) will need to be calculated based on safety categories that are established in line with factors such as a measure of diagnostic capabilities (DC) for the control system, the meantime to dangerous failure (MTTFD) and common cause failure (CCF). In combination, these inputs will define the level of a given safety function.
In tandem with the strategy set out here, peace-of-mind can, of course, be found by specifying safety-rated products from a reputable supplier. After all, as machine builders will be well aware, the price of non-compliance can be extremely costly.
To discover more about Parker’s factory automation solutions, please see our guide "A Comprehensive Guide to Machine Safety".
Article contributed by Linda Caron, global product manager for Factory Automation, Pneumatic Division.
Related content
Understanding the Machinery Directive
Know Your Pneumatics: Safety Exhaust Valves
4 Ways to Achieve Required Safety Levels with Pneumatic Exhaust Valves
Industrial Ethernet (IE) is growing at a startling rate. In fact, the latest estimates put the annual growth at a staggering 22 percent, which means some 52 percent of the connectivity market is now commanded by IE, putting it ahead of traditional fieldbus networks for the first time.
There are many reasons for this. In our opinion, these include the widespread accessibility of several IE protocols, a good degree of backward compatibility and the availability of rugged components (hardwired) that are typically protected from electrical noise. And it is important to not overlook the emergence of cloud technologies, as well as the pure and simple demand for more connected devices as part of industry’s smart factory evolution.
Smart factories look to eliminate downtime and enhance productivity, which is why the systems and equipment in such facilities must be far more intelligent, flexible and dynamic.
Data collection and analysis is at the core of this effort, an activity that is intended to aid faster and more informed decision making. It’s perfectly clear why all of you production managers out there would want to make decisions based on accurate reporting of what’s actually trending on the shop floor.
From a technical perspective, analytics can be accomplished in different ways. Data can be stored and retrieved as needed (acyclic data) or returned through the network in real time for immediate attention (cyclic data).
In either case, as already mentioned, there are numerous IE protocols which can help communicate this data, not least familiar ones such as Profinet, Ethernet /IP and EtherCAT. And each has its own set of attributes, but regardless of which best suits a given application, the proliferation of these protocols has made IE a major fixture in control systems around the globe.
While our industry is without doubt seeing more take-up of IE, the goal for automation equipment vendors has been delivering IE connectivity in a cost-effective and straightforward manner. For this reason, Parker has been busy developing a high-capability, high-reliability IE network node: the P2M node.
Designed with advanced factory automation in mind, Parker’s engineers have created the node so that it’s both easy to configure and cost-effective. The result is that the company’s H Universal ISO Series valve, Moduflex valve and H Micro valve families can now connect to the IE network. In fact, we can now offer a large range of IE connectivity options, including EtherNet/IP, Profinet IO, EtherCAT, Ethernet PowerLink, Modbus TCP/IP and CC-Link IE protocols.
Adding further to the options for easier and more cost-effective network connectivity is our H Series Network Portal, which delivers on-machine flexibility for IE applications. The portal handles machine digital or IO-Links I/O's, eradicating the necessity for extra PLC input and output cards or other remote I/O modules. Offering full configurable IO-Link channels on the valve manifold via the network portal facilitates straightforward and cost-effective centralised machine application, even in caustic, wash-down or hazardous areas and even where extreme temperatures are present.
Ultimately, the reality of low-cost connectivity with integrated diagnostics has at last arrived, serving to further reduce complexity and cost at the machine, while simultaneously meeting the requirements of smart factories and Industry 4.0. The IE compatibility of critical automation components such as pneumatic valves is paramount if industrial users are to leverage the full benefits that total and reliable connectivity can bring.
Learn more
If you’d like to discover more about Parker’s P2M IE network node, please watch the video below:
Article contributed by Patrick Berdal, EMEA product manager for control devices, Pneumatic Division Europe, Parker Hannifin Corporation.
Related content
Achieving Simple and Cost-Effective Industrial Ethernet Connectivity
Optimise your Connection of Pneumatic Manifolds to Industrial
Networks What is the Foundation for a Smart Factory?
Careful and correct sensor installation is vital if accurate and reliable information is to be measured and communicated from the sensor.
What all engineers want when it comes to sensor installation is a simple, secure and rapid assembly process, without complicated processes such as the need for additional mountings.
The P8S proximity sensor offers universal use, flexible integration and excellent form. Its square design is also suitable for rapid installation in industry-standard T-slots, regardless of cylinder profile or brand. The upshot of this direct, drop-in design – as opposed to ‘turn-in’ or ‘slide-in’ concepts – is a significant reduction in installation time.
Among the innovations with the P8S are retaining ribs on the side of the sensor body that enable simple mounting, including hard-to-reach locations or overhead assemblies. These ribs ensure the sensor conveniently holds its position in the T-slot even before the screw is tightened.
To begin the installation, simply slide the sensor into the T-slot. When in the desired position, a quarter-turn of the eccentric stainless steel screw is all that is required to secure the sensor. To further simplify mounting, the screw head design is such that it accepts either a flat-blade screwdriver or Allen key. The mounting screw even features a knurled head that helps to withstand shock or vibration.
Of course, not all cylinders have T-slots. With P8S sensors this is not a problem as they also mount externally to cylinders. As a result, fitment to round, tie rod and profile cylinders are straightforward.
To make life as simple as possible, every P8S sensor is delivered with a specific adaptor to suit dovetail grooves. Also available are special brackets for round and tie-rod cylinders. The concept is to provide one sensor for all actuator types and brands - not just Parker units.
Cables are be supplied in three or 10 metre lengths (flying lead) or 0.3 metres with an M8 rotating plug, as standard.
Ultimately, automation demands excellent functionality and precision, which in turn requires solid expertise and knowledge at all levels, including best-practice installation.
Learn more
To discover more about Parker P8S sensors and benefits they can deliver, watch this video:
This article was contributed by Franck Roussilon, product manager, Pneumatic Division Europe, Parker Hannifin Corporation.
Related content
Three Things to Consider When Choosing a Smart Sensor
Easy Steps to Installing and Configuring a CPS Sensor
Know Your Pneumatics: Continuous Position Sensing
How to Install Pneumatic Cylinders to Maximise Life and Performance
Know Your Pneumatics: Selecting a Pneumatic Cylinder | Operating Environments