• Home
  • Investors
  • Contact Parker
  • Sign In / Register
Parker Community
  • Site
  • User
  • Site
  • Search
  • User
  • Products
  • Support
  • Divisions
  • Where to Buy
  • Careers
  • About Parker
Home Parker Community Technologies Process Control
Sign In / Register

Sign In

Register

  • Home
  • All Blogs
  • Home
  • Process Control Blog
  • Process Control Forums
  • Process Control Knowledge Base
  • Process Control Members
  • Mentions
  • Tags
Twitter
Tweets by @ParkerProcess

Follow Us
  • Follow Parker Hannifin on social media

Follow Parker Hannifin on social media:

Process Control

Process control is the technology of regulating processes to provide stable and consistent output. Parker strengths include process instrumentation, semiconductor, power generation, medical and analytical applications.

Process Control Managers:

Gemma Steele
Charles Harris
Browse Knowledge Base
  • Process Control Knowledge Base

    32 pages
Latest Blog Posts

Why Making the Right Tube Connections for LNG Plants is Vital - Tube connection - Parker HannifinSmall and mid-scale LNG plants are dramatically changing the application sphere for natural gas as an alternative fuel for transportation, both onland and for marine shipping use. They are helping drive adoption in various high horsepower applications and making gas capture and distribution from remote areas and wells without pipelines a reality.

LNG plant requirements drive need for smaller line and fittings

As the requirement for small and mid-scale LNG plants grows, so does the need for tube connection technology for smaller line sizes. In the past, connection technology was limited to either orbital welding or double ferrule compression fittings. Today, driven by cryogenic applications, there are four connection options in the less than two-inch space: instrumentation compression double ferrule fittings; instrumentation compression single ferrule fittings; O-ring face seal fittings; and permanent fittings.

Connection in a cryogenic application should focus on five critical areas:

  • Safety
  • Leakage and fugitive emissions
  • Ease of assembly
  • Longevity
  • Code compliance
Safety first

Safety is critical in small and mid-scale LNG plants. In these complex plants, electricity, gas and water will often coexist in close proximity. Add cryogenic temperatures to the mix and the environment becomes extreme.

The most important rule of safety in an LNG plant is to keep the media contained. Good tube connections prevent catastrophic failure at connection points. A failure mode and effect analysis reveal the threat that a bad connection – or a poorly made one – can pose to a plant. In addition to explosion leaks, the danger of frostbite exists with cryogenic temperatures. A good connection is a first defense in preventing exposure and harm to personnel.

Leakage and fugitive emissions

Leakage of methane, a greenhouse gas -- while still not regulated -- is a major concern in LNG plants. Overall, fugitive emissions will become increasingly important; keeping hundreds and thousands of connections in an LNG plant from leaking will be key.

As a basic requirement, ensure bubble-tight connections that follow appropriate leak specifications to future-proof against fugitive emissions while not limiting solely to safe exposure levels. Apart from methane leaks, cryogenic fluid leaks can cause frostbite and major freezing hazards. A small, seemingly safe leak is also a loss of revenue and efficiency. Leak-tight connections can add up to savings and notable percentage points of efficiency.

Ease of assembly

A big challenge for small-scale, modular LNG plants is the flexibility to connect on-site to a dispensing system or a point-of-use system. This often means a lot of field connections and the capability to carry out repairs. Other times it means making certain connections at the time of installation. While welding sometimes seems to be the most straightforward strategy for a permanent joint, finding certified and trained welders may not be simple or easy.

Longevity

With the operational life of an LNG plant in the range of 15 to 25 years or more, it is critical to select corrosion-resistant, robust and reliable connection technologies that outlast the moving parts. Longevity can be achieved by choosing materials that resist corrosion from environmental sources and that are compatible with the media or fluid being transported.

Code compliance

Finally, it is essential to consider applicable codes of construction that, in some environments, may include marine standards such as those for ABS or DNV GL. Code compliance helps ensure that all the above topics are covered. Codes to consider include:

  • In the US: NFPA 59A
  • In Europe: EN 1473:2007 and EN 13645
  • Globally: ISO (draft) 116901, ISO TC 67, ISO 18638, ISO TC 252

The end-use must take into account all possible interface points such as vehicles, tankers, vessels or rail cars to define application standards.

Connection technology challenges and advantages
  • Why Making the Right Tube Connections for LNG Plants is VitalThe double ferrule compression fitting is a well-known component to most fitters in the industry. A single ferrule fitting allows the use of the same skill set as a double ferrule fitting but reduces the risk of making a wrong connection since one ferrule is eliminated. Both types provide good field make-and-break capability.
  • The O-ring face seal fitting and flanged tubes may be tightened and remade many times, and to set torque, provide zero-clearance tube entry. Additionally, the metal seal ensures LNG compatibility.
  • Finally, the permanent fitting can replace a normally welded joint or a fitting joint that typically would never need to be reopened in the field. A permanent fitting can also be made much faster and without field orbital welding.
Better protection against fugitive emissions

In both single and double ferrule fittings, stainless steel parts that rub together under high pressure have a strong tendency to cold weld and seize, leaking to leaks and the resulting fugitive emissions.

Using fittings coated with molybdenum disulfide can avoid this problem. Solid molybdenum disulfide readily adheres to surfaces, is noted for its lubrication and anti-seizing properties, and does not squeeze out under extreme pressure. The result is low assembly torque and consistent, leak-free performance, even with repeated remakes.

Many fittings manufacturers also combat fitting leaks – and the resulting possibility of fugitive emissions – through proprietary ferrule-hardening processes designed to heighten corrosion resistance. For example, Parker treats its ASTM 316 stainless steel, single and double ferrule fittings with Suparcase®. The chemical process provides greater resistance to pitting, as well as excellent stress corrosion performance to provide longer, leak-free service life.

 

Article contributed by the Process Control Team. Original article published at LNG Industry in September 2015.  

 

Related articles on Alternative fuels - CNG and LNG:

Transportation Fuel - LNG OR CNG?

How New LNG and Natural Gas Fuel System Architecture is Advancing the ‘Golden Age of Gas’

The Choice Between LNG and CNG as Transportation Fuel

Parker Complete Piping Solutions Receives ASME B31 Compliance

Is It Safe to Mix Compression Style Instrumentation Tube Fittings?

Manifold Connector Technology – Why Settle for Second-best?

How to Avoid H2S Embrittlement in Instrumentation Connections

 

Why Making the Right Tube Connections for LNG Plants Is Vital

14 Jan 2021

Read more

Molybdenum Disulfide- Optimizing Leak-Tight Compression Fitting Performance - Power plant - Parker HannifinIncreasing customer demand requires new process applications with needs for reliable lubrication and resistance to galling under stringent conditions of temperature, pressure, vacuum, corrosive environments, process sensitivity to contamination, product life, and maintenance requirements. The various applications within power generation and industrial and chemical processing have advanced lubrication needs. Specifically, this blog is related to the science of molybdenum disulfide coatings in compression fittings. In demanding environments, such as power generation plants, where tubing connections are exposed to stringent requirements and extremes, consistent leak-tight performance is critical and molybdenum disulfide coated fittings provide a solid solution. 

 

Lubrication evolution increases demand

 Molybdenum disulfide is a naturally occurring black colored solid compound that feels slippery to the touch. It readily transfers and adheres to other solid surfaces with which it comes into contact. Its mineral form – called molybdenite – was commonly confused with graphite until late in the 1700s. Both were used for lubrication and as writing material for centuries. Wider use of molybdenite as a lubricant was impeded by naturally occurring impurities that significantly reduced its lubricating properties. Methods of purifying molybdenum disulfide and extracting molybdenum were developed late in the 19th century, and the value of molybdenum as an alloying addition to steel was quickly recognized. The demand for a domestic source of molybdenum during World War I resulted in the development of the Climax mine in Colorado, which started production in 1918 and continued into the 1990s.

The availability of high purity molybdenum disulfide spurred extensive investigations into its lubrication properties in various environments during the late ’30s and ’40s. These investigations demonstrated its superior lubrication properties and stability under extreme contact pressures and in vacuum environments. These investigations resulted in extensive applications in spacecraft.

 Download our white paper Molybdenum Disulfide - The Ideal Solid Lubricant and Anti-Galling Material for a closer look into the science behind high-performance compression tube fittings required for demanding environments.

 

Exceptional lubricity

 Molybdenum disulfide’s exceptional lubricity is a consequence of its unique crystal structure, which is made up of very weakly bonded lamellae. The lamellae tend to align and adhere to contact surfaces, particularly under conditions of sliding and pressure, as shown here. This “burnishing in” of the molybdenum disulfide gives it its exceptional performance life.

 

 

Since molybdenum disulfide is a solid phase, it is not “squeezed out” like liquid lubricants under conditions of extreme pressure. The lamellae are very “hard” to forces perpendicular to them. This combination of properties provides a very effective “boundary layer” to prevent the lubricated surfaces from contacting each other.

 The surfaces of objects are generally rough on a microscopic scale. When two objects are in contact with each other, they actually “touch” at very small regions of contact (i.e., asperities).

 

 These contact regions have considerably less area than the bulk surface area, typically in the range of 0.5 to 0.001 percent of the bulk area for a machined metal surface, and consequently, the stresses at these contact points are considerably higher than the stresses calculated for the bulk surface area. When these objects slide relative to each other the frictional forces add to the stresses at the contact points, and the resultant stresses may be sufficient to cause deformation of the contact points.

When stainless steel objects slide against each other under high load, they will “gall” or “seize” due to the deformation at the contact points. The objects will actually “cold weld” themselves to each other, which is indicated by the transfer of material from one object to the other on the sliding surfaces. This causes a very rapid increase in friction, quickly to the point that further sliding is impossible without damage to the objects. To prevent this, it is necessary to introduce an “anti-galling” or “anti-seizing” agent between the surfaces. This is a substance that can maintain separation of the surface asperities under high compressive loads – that is, to provide a “boundary layer” between the surfaces. Anti-galling materials are generally very thick grease-like substances or solid materials in powder or plated layer form. Molybdenum disulfide is an ideal anti-galling compound because of its combination of high compressive strength and its adherence (ability to fill or level) to the sliding surfaces.

There are many methods of applying molybdenum disulfide to a surface, from “high tech” techniques such as vacuum sputtering, to simply dropping loose powder between sliding surfaces. The most versatile technique is the application of the powder mixed with a binder and a carrier to form a bonded coating. The binder may be a polymeric material or several other compounds, and the carrier may be water or a volatile organic. The characteristics of the molybdenum disulfide powder, the binder, the carrier, and particularly the application process must be carefully developed and controlled to optimize the performance of a specific product. A properly developed bonded coating of molybdenum disulfide can provide exceptional lubrication performance over a temperature range up to approximately 500°C, under very high pressure and corrosive exposure conditions for extensive lifetimes.

 

Molybdenum disulfide in compression fittings

During fitting make-up, the ferrule(s) is driven forward into the body seat and tubing surface as the nut is turned per the makeup instructions. The ferrules seal at contact points with the fitting body seat and tubing surface. The fitting is carefully engineered such that the ferrule and tubing do not rotate with the nut, moving only in the axial direction. This is critical to forming a high integrity leak-free tubing connection during the first make-up and subsequent remakes. Therefore, the sliding takes place between the back of the ferrule and the flange of the nut under very high pressure. This region of contact between the nut and the ferrule must have excellent lubrication for the proper action to occur during make-up to ensure ease of assembly, low make up torques, and optimum fitting function. The nut is “pulled” against the ferrule during make-up by the threads, which are also sliding under very high pressure and require high-performance lubrication.

Stainless steel compression fittings have the additional problem of preventing galling in these areas of sliding under very high contact pressures. This requires a “boundary layer material” – a substance that maintains separation of the surfaces during sliding.

Our instrumentation engineers have developed and used a bonded molybdenum disulfide coating on the nuts of our premium CPI™ compression fitting products for 30+ years. These fittings are readily recognized in the field by the “black nut” – the molybdenum disulfide coated nut, and have been providing exceptional service in many demanding applications.

The molybdenum disulfide coating has been carefully formulated and processed to optimize the performance of the CPI™ compression fitting. This fitting, with its single ferrule and the molybdenum disulfide, coated nut, has easy initial make-up with very low torque, consistent remake, and exceptional, leak-tight performance under demanding power generation applications including pressure, temperature, corrosion exposure, and vibration.

 

One product, multiple applications

We also offer a “Moly Inside” nut for use with our CPI™ and A-LOK® compression fittings. This is an optional version of our premium compression fitting products with the molybdenum disulfide coating only where it is needed, on the inside surfaces of the nuts. This offers the same low make-up torque and consistent remake-ability of the standard CPI™ compression fitting in both the CPI™ and A-LOK® versions due to the use of molybdenum disulfide on the critical mating surfaces of the interior threads and flange of the nut, but without the molybdenum disulfide on the external surfaces to rub off onto hands, gloves, or other equipment for industries requiring a “clean” appearance.

 

 Download our white paper Molybdenum Disulfide - The Ideal Solid Lubricant and Anti-Galling Material for a closer look into essential attributes of high-performance compression tube fittings required for extreme environments.

 

 

 

 

 

 

Molybdenum Disulfide- Optimizing Leak-Tight Compression Fitting Performance- Kevin Burke - marketing manager Parker HannifinArticle contributed by Kevin Burke, marketing manager, Instrumentation Products Division, Parker Hannifin.

 

 

 

 

Related, helpful content for you:

Safe Power Generations Solutions for Global Demand

Defining Our Unique Contribution to the World

Metallurgy Makes or Breaks Tube Fittings

Why Choose Single Ferrule Tube Fittings for Vibration Protection and Temperature Cycling

Reduce Combustion Gas Turbine Downtime with Leak-Free Extreme Temperature Fittings

Faster Tubing Connections for Medium Pressure Applications

Molybdenum Disulfide- Optimizing Leak-Tight Compression Fitting Performance

12 Jan 2021

Read more

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_Heavy-duty trucks_Parker Hannifin, Instrumentation Products DivisionIn the quest for a decarbonised society there is no doubt that Hydrogen as an environmentally friendly fuel source is gaining a lot of popularity to become the fuel of the future. And the hydrogen revolution is happening now. Driving the ecological transition, hydrogen-based technologies are rapidly evolving, mass entering the market and becoming part of our daily lives. From clean power generation to environmentally friendly cars, the possibilities are endless.

The transportation sector is a prime example of how hydrogen technologies are taking off and making truly sustainable mobility more tangible than ever. Heavy trucks with hydrogen-powered cells are already hitting the roads, and although developing a global hydrogen refuelling infrastructure might take several years or even decades, the commitment to hydrogen economies from governments all around the world will certainly accelerate its pace.
 

 Download our white paper: Addressing the Challenge of Hydrogen Embrittlement in Metallurgy.

 

 

 

 

 

The hydrogen challenge

Hydrogen is the most abundant element in nature and its versatility can offer compelling advantages as an accessible, sustainable and efficient alternative source of energy.

However, hydrogen can be very damaging to most metallic materials, causing what is known as hydrogen damage or hydrogen attack. Hydrogen is an extremely small particle and hydrogen degradation is directly connected to its capability to be easily absorbed by metals coupled with the high mobility those particles have at microstructural level.

Nearly every metallic material can be susceptible to hydrogen damage, and there are several forms of hydrogen degradation. Hydrogen embrittlement cracking is the most common form and affects the three main areas of industries that use hydrogen:

  • Production
  • Transportation
  • Storage
  What causes hydrogen embrittlement? Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_Hydrogen_Embrittlement_Parker Hannifin, Instrumentation Products Division

Fig. 1. Embrittlement process.

Embrittlement occurs when a material loses ductility and becomes brittle as a result of the diffusion of hydrogen into the material. The hydrogen atoms find preferential places in the structure of the material, modifying its physical properties and its mechanical behaviour. The result is a loss of ductility which makes the material more brittle and more susceptible to cracking. Hydrogen can be a silent assassin, weakening the material slowly and without any clear signs of damage, often leading to critical failure.

 

The effect of hydrogen embrittlement is determined by three main challenges:

 

  • The Environment
  • The Mechanics of the material
  • The Microstructure characteristics of the material.

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_Hydrogen_Embrittlement_elements_Parker Hannifin, Instrumentation Products Division

Environment

Hydrogen and stress need to be present on a susceptible material for hydrogen-assisted fracture to happen. Firstly, hydrogen absorption can happen at both production and service stages. Processes such as uncontrolled melting, electroplating or welding can promote the pre-charge of hydrogen into a given metal.

Microstructure

In terms of microstructure, and as a rule of thumb, materials that bestow high mechanical strength or show a great number of defects and inclusions are likely to be more susceptible to this type of failure. The severity of hydrogen embrittlement is also a function of the operating temperature, with low temperatures being the worst case scenario in terms of material ductility and higher temperatures in terms of hydrogen absorption rate.

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_Hydrogen_Crack_Parker Hannifin, Instrumentation Products DivisionThe factors that can affect the quality of the microstructure are numerous and have been widely documented by the materials society. Due to the complexity of the subject, the effect of microstructure as a major contributing factor to hydrogen behaviour, cannot be evaluated in simplistic terms. Taking one variable in isolation is not enough to guarantee the quality or performance of a given component and can be misleading. For example, a material grade with a ‘perfect chemistry’ or with high levels of a particular ingredient can still result in a very low quality product.

The common consequences of improper and non-controlled material processing, heat treatment and/or manufacturing operations are high densities of undesirable phases and inclusions in the raw material. These will inevitably lead to fatal and premature hydrogen assisted cracking during service in demanding H2 environments.

Application mechanics

The mechanics of the application also play a major role. Stress states in components can be caused by the presence of residual stresses associated with certain fabrication techniques as well as stresses applied during service. Improper product design and improper installation can cause overloading of stress onto the material. All of these factors can cause premature failure of components in Hydrogen service.

Can hydrogen embrittlement be prevented?

When it comes to handling hydrogen, material and equipment selection becomes, more than ever, an essential ingredient for success.

According to the International Industry Standard ISO 15916-2015, due to the fact that most metals are susceptible to different levels of H2 embrittlement, materials of construction and suitable equipment must be carefully selected to avoid failure when hydrogen exposure is anticipated. The positive news is that hydrogen embritllement can be prevented. End users need to pay special attention to the materials of construction and the quality of the equipment that goes into their assets.

How Parker is at the front end of innovation for the hydrogen market

As a manufacturer of pressure containing equipment, Parker has decades of experience in serving hydrogen applications. Parker products are designed to minimise the risk associated with corrosion and hydrogen attack and deliver successful performance in the field. The raw materials that we use are fully traceable and closely controlled from melting stage to the finished product.

In addition, our manufacturing processes are selected to ensure minimum operating risk in hydrogen environments. As well as Stainless Steels (the prime material of choice for the H2 transportation sector), we can offer a variety of nickel alloys for a wide range of other applications.  

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_A-LOK_Fittings_EC-79 Approved_Parker Hannifin, Instrumentation Products Division

Parker's portfolio also includes EC-79 approved products. The EC-79 approval (the Regulation of the European parliament and the Council of 14th January 2009 on type-approval of hydrogen powered motors) is an EU normative for components and systems which are installed on hydrogen-driven vehicles. Product ranges certified to this regulation are extensively tested to guarantee the safety and performance of H2 equipment under different pressures, electric, mechanical, thermal or chemical conditions.

As a leading manufacturer in motion and control technologies Parker offers a wide range of products orientated to the hydrogen market. 

 

 

Fig. 4. Parker A-LOK® two ferrule tube fittings

EC-79 approved for use on-board hydrogen vehicles up to 350 barg pressures.

 

 Download our white paper and learn the main causes of hydrogen embrittlement and best practices on how to prevent it. 

 

 

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy_Clara_Moyano_Parker Hannifin, Instrumentation Products Division

Article contributed by Clara Moyano, innovation engineer - Materials Science, Parker Hannifin, Instrumentation Products Division Europe.

 

 

 

 

 

Related content:

Instrumentation Solutions for Hydrogen-Powered Vehicles

Learn How  Parker Supports the Transportation Industry

How to Avoid H2S Embrittlement in Instrumentation Connections

Materials Selection: Choosing the Right Mix to Prevent Corrosion in Your Installation

Metallurgy Makes or Breaks Tube Fittings

Mixing Materials in Corrosive Environments

Addressing the Challenge of Hydrogen Embrittlement in Metallurgy | White Paper

16 Dec 2020

Read more

Clean Transportation for a Sustainable Future - Infographic on CNG LNG Hydrogen - Parker HannifinOf the many transport fuel choices available today, none plays a more strategic role than natural gas in having an immediate and major positive economic and environmental impact. But of the two most widely available – CNG and LNG – which is most appropriate?

 

 

  Onboard vehicle filling stations  - Compressed Natural Gas

Compressed Natural Gas (CNG ) is a fuel produced by purifying natural gas and cooling it to less than 1% of its volume and stored onboard a vehicle in a compressed gaseous state at a pressure of up to  3600 PSI. CNG is used in light-, medium, and heavy-duty vehicle applications.

  Gas transport and storage - Liquidized Natural Gas

LNG is a fuel produced by purifying natural gas and cooling it to -161°C to turn it into a liquid. LNG is suitable for trucks that require longer ranges and typically used in heavy-duty vehicles. Parker Bestobell’s cryogenic valves are widely used on road LNG trucks transporting LNG to fueling station sand storage tanks. 

 

On-board vehicle filling station - Hydrogen 

Hydrogen can be produced from fossil fuels, biomass, and water electrolysis with electricity. The environmental impact and energy efficiency of hydrogen depends on how it is produced. Hydrogen-powered vehicles work by converting compressed hydrogen from their fuel tanks into electricity that powers their engines. This process generates only water vapor and heat emissions.

  Solutions
  • Fittings and tubing - Parker’s A-LOK® two ferrule fittings, CPITM single ferrule fittings and tubing provide reliable leak-free tube connections on-board CNG vehicles and at fueling stations. The unique SuparcaseTM hardened ferrule design provides superior grip and safe lifetime operation.
  • CNG valves and pressure regulators - Parker’s high integrity precision ball valves Hi-Pro® and B Series, check valves and pressure regulators provide safe isolation, regulation and control onboard CNG vehicles and at fueling stations. 
  • Fuel regulation module - Parker’s integrated gas regulator system, FM80 provides advanced fuel handling performance. Piston regulator design delivers better control, fewer connections, and longer range.
  • Cryogenic safety relief valves - Parker Bestobell’s cryogenic safety relief valves are designed to protect LNG storage tanks or capital equipment on road-going transport trucks from damage caused by over-pressure.
  • LNG Cryogenic check valves - Parker Bestobell’s cryogenic check valves with innovative loose flange bolted bonnet design allow for thermal expansion and contraction eliminating leakage and maximizing safety and performance.
  • Cryogenic globe valves - Parker Bestobell’s cryogenic globe valves deliver smooth operation and reduced closing torque by use of a PTFE anti-friction disc between the valve spindle and the disc assembly.
  • Fittings - Parker’s A-LOK® two ferrule fittings up to 1” size provide reliable leak-free tube connections onboard hydrogen-powered vehicles and at fueling stations. The unique SuparcaseTM hardened ferrule design provides superior grip and safe lifetime operation. EC-79 approved.
  • Medium pressure valves - Parker Autoclave Engineers needle valves, check valves, filters utilize a coned-and-threaded connection design providing a leak-tight reliable connection at fueling stations in applications up to 20,000 PSI and temperatures from -73° to 316°C.
  • Medium pressure tubing and fittings - Parker Autoclave Engineers medium pressure cone & thread fittings provide reliable leak-free and safe lifetime operation at fueling stations.

 

 

Alternative fuel solutions for trucks and buses contribute to a better world.

Alternative fuels (CNG, LNG, H2 ) are emerging as strong and viable alternatives to traditional fuels for HGVs for many reasons: energy security, economics and the potential to reduce emissions and noise. Parker’s solutions for reliable fuel distribution and regulation help OEM’s around the world drive towards a better future.

Contributed by the Process Control Team.

Related alternative fuel content:

Parker Helps Guarantee Safe Refueling at New CNG Bus Filling Station in Azerbaijan

Certified Natural Gas Vehicle and Fueling System Products

The Importance of Natural Gas Product Certifications

The Choice Between LNG and CNG as Transportation Fuel

New CNG Bus Filling Station Guarantees Safe Refueling

Seal-Lok ORFS CNG Fittings Pass On-Vehicle Fire Safety Test

CNG Fuel Systems for Heavy Duty Vehicles

How New LNG and Natural Gas Fuel System Architecture is Advancing the ‘Golden Age of Gas’ Parker Helps Guarantee Safe Refuelling at New CNG Bus Filling Station in Azerbaijan

Leading CNG Provider Implements PTS to Reduce Costs and Improve Ordering Levels

The Route to Reliability - How to Specify the Right Product for Transport Safety and Performance

 

 

Clean Transportation for a Sustainable Future | Infographic

4 Dec 2020

Read more

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Installation_Corrosion on SBT Systems_Parker Hannifin_Instrumentation Products Division Corrosion is a major challenge for many design engineers and specifiers in the general industrial market. Choosing the right materials is critical to ensure optimal performance, as even the highest quality products can fail if not used properly.

 

Materials selection: three key questions to answer

Engineers must carefully analyse the proposed operating environment when selecting materials for industrial applications. Answering three important questions will help unearth potential problems and provide useful guidance on appropriate materials to use.

 

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Installation_Factors to consider to minimize Stress Corrosion Cracking_Parker Hannifin_Instrumentation Products Division

Fig. 1 Materials selection: factors to consider to minimize Stress Corrosion Cracking (SCC)

The three questions to consider are:

Q1. Is the material composition susceptible to cracking?

As this diagram shows, if potentially corrosive media (such as chloride containing compounds) needs to be contained and the material is susceptible to cracking, corrosion can occur. Material susceptibility is not purely about chemistry, though; factors such as material processing, specific microstructure and surface condition are also important.

Q2. Is the application environment potentially corrosive?

Environmental factors can include a range of parameters – chemical composition, flow rate, temperature, or electrode potential, which can be aggressive and lead to
corrosion and cracking.

Q3. Is the material concentrated load under tensile stress?

Stress can be imparted into a component in various ways – from service stress and vibration to residual stress derived from manufacturing processes or heat treatment.

Answering these questions helps to build a picture of what is appropriate for the individual circumstances. A small investment of time upfront can make a big difference to the longer-term success of an installation.

Find out more about material selection and what to consider, in this video featuring Parker’s innovation engineer for material science.

 

Materials selection and cost-efficiency

If a specific mix of materials was used successfully for a previous project, it can be tempting to rely on what has gone before. But that is not always a good idea.

With more than 300,000 product materials to choose from, materials selection presents a big challenge for many specifiers. It’s easy to feel spoilt for choice or be overwhelmed by the range of options available. But adding extra elements can complicate things… sometimes, just one material might be enough for the job! It’s important to know when adding a small amount of an element could increase costs, without any obvious customer benefit.

Conditions in many industries have changed; and it’s important to keep adapting materials to reflect this. Climate change is also key. For example, if summer temperatures have raised by a few degrees, some materials suitable in the past may no longer be appropriate.

It’s worth bearing in mind that:

  • Cheaper initial costs aren’t necessarily the most cost-effective option
  • There’s a difference between what is technically possible, and the best solution for installation.

Not all alloys are created equal, and even identical chemistries can lead to different final products. Parker’s 316 stainless steel A-LOK® tube fittings with min. 10% of nickel content has operated successfully in critical applications for 50+ years.

Good steel combines chemistry and processing. Parker tightly controls all specifications in terms of raw material quality, corrosion performance, mechanical properties, and heat treatment. Production routes are controlled from melting to a machined product; this ensures that customers get the best possible performance for their applications and a material that offers full traceability.

 

Managing risk when mixing materials

To get optimal results from your budget, it’s helpful to use the best material for the job, at the lowest possible cost. But when budgets are under pressure, some engineers may mix alloys on the same application.

Although using dissimilar materials seems like an easy way to save costs, it can be risky. Just because something looks strong and resilient, doesn’t mean that it will last for a long time. And mixing dissimilar materials for instrumentation can lead to SCC, where localised attacks at one point gradually progress to other areas of the system. SCC can lead to fatal failures.

NORSOK Standard M-001 Materials Selection states that

“‘At galvanic connections between dissimilar materials without isolation, it can be assumed that the local corrosion rate near the interface is approximately 3 times higher than the average corrosion rate. Particular systems may have higher corrosion rates depending on area ratio and material combinations.”

If a proposed application is highly demanding and requires expensive material, that’s likely to be important across the whole system. Ultimately the whole system operates in the same environment, contains the same media, and operates at the same pressure; therefore, it makes sense to use the same material throughout, rather than (say) using one material for the tubing and another for fittings.

Not everyone has access to a materials expert with their projects, but Parker’s specialist metallurgists bring many years of experience. This helps engineers identify the best materials for an application and predict likely failure risks. For example, using 316 stainless steel in seawater may not be a good choice because it is more susceptible to corrosion; but alternatives such as super austenitic stainless steel 6Mo (UNS S31254) or nickel alloy C276 (UNS N10276) may work, as they are designed to withstand chloride-containing environments with greater resistance to pitting or crevice corrosion.

 

Improving engineer confidence and skills with SBEx training

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Installation_SBEx Small Bore Expert training_Parker Hannifin_Instrumentation Products Division For some customers, specialist training provision can reduce the likelihood of potential fitting failures. For example, Parker’s Small Bore Expert (SBEx) training provides valuable guidance on correct fitting assembly and material selection. Suitable for fitters, technicians, and maintenance personnel, this course helps organisations to save time, reduce overheads, and increase safety.

 

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Installation_ Download Brochure_Parker Hannifin_Instrumentation Products DivisionDownload our brochure with tips on smarter materials selection for corrosion control.

 

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Installation_Clara Moyano Innovation Engineer - Materials science_Parker Hannifin_Instrumentation Products Division Article contributed by Clara Moyano, innovation engineer - Materials Science, Parker Hannifin, Instrumentation Products Division Europe

 

 

 

 

Related Content:

Smarter Materials Selection for Corrosion Control - Download Brochure

How to Avoid H2S Embrittlement in Instrumentation Connections

Mixing Materials in Corrosive Environments

Metallurgy Makes or Breaks Tube Fittings

Understanding Corrosion in Challenging Offshore Applications

Materials Selection: Choosing the Right Mix to Prevent Corrosion in your Install...

7 Oct 2020

Read more

Best Practices for Dust Suppression in Underground Coal Mines - Coal Mining Site - Parker HannifinPrevention is better than a cure. In coal mining, these words offer particularly good guidance. Underground mining presents numerous hazards ranging from structural collapses, flooding and explosions. The tremendous amount of dust generated by activities in a coal mine creates breathing-related problems for workers as well as maintenance issues for machinery. Dust can also create a potentially explosive environment. Injuries and deaths occur every year either from accidents or health issues caused by exposure to coal dust. Mining companies can dramatically reduce these risks by applying rigorous dust suppression safety measures.

This blog investigates dust suppression methods and evaluates preventative versus corrective techniques that can effectively be used to suppress dust in underground coal mines, reducing the risk to workers and equipment.

 

Best Practices for Dust Suppression in Underground Coal Mines - Download the white paper, the Science of Dust Suppression - Parker Hannifin

 

 

Download the full white paper “The Science of Coal Dust Suppression” for technical details and additional information on preventative coal dust suppression.

 

 

 


The dangers of dust

Coal dust is a known carcinogen that causes miners’ lung disease (pneumoconiosis). Dust in the atmosphere can also create an ignition hazard when mixed with gas. Coal dust buildup is often a root cause of premature maintenance and failure of mining equipment. To this end, preventative suppression is critical.


Dust suppression methods

There are a variety of ways to suppress dust in coal mines that offer a varying degree of effectiveness and efficiency. The most common methods are: 

  • Bag filter system
  • Dry fog system
  • Use of water

Bag filter system uses fans to circulate the air and trap the solids in a bag. However, this type of system is maintenance-intensive and requires bag filter change-outs — which is not conducive to work in an underground mine.

Dry fog system requires electricity, making it impractical for work below ground level.

Water is an ideal solution because it takes advantage of the mine's existing water supply, forming it into a spray to suppress the dust as soon as it is generated at the coal extraction point and all other areas where dust is generated.

 

Preventative vs. corrective dust suppression using water Preventative dust suppression

Logically, if a problem can be prevented from happening, then the time and cost of fixing it can be saved. Preventing dust from becoming airborne is critical in dust suppression. Three important elements to successful preventative suppression using water include:

  • Control
  • Filter 
  • Spray

Control pertains to how the water is controlled. It may be controlled by the presence of coal on the conveyor or by the belt’s motion. In either case, the water is isolated before entering the system.

Filter technology is used to remove contaminants from the water to assure reliable system operation.

Spray refers to a predetermined volume and pattern in which the water is delivered to the coal before the dust is generated.

The figure below shows a typical belt conveyor transfer point dust suppression system has two options: paddle valve (A) or belt-driven valve (B). Both are designed to operate only when there is coal on the conveyor.

Best Practices for Dust Suppression in Underground Coal Mines - typical belt conveyor transfer point dust suppression system - Parker Hannifin


Corrective dust suppression 

Corrective or symptomatic dust control is implemented after the dust is created and is more challenging than preventative dust control. Dust particles come in a range of sizes with some as small as 10 µm which is invisible to the human eye. These small particles are the most dangerous to workers and equipment because they can remain airborne for long periods of time and eventually find their way into miners’ lungs, onto and into machinery as well as outside of the mine itself. Small particles are also the most difficult to remove from the atmosphere. Airborne coal dust can be addressed correctively using sprays. The principal is that the dust agglomerates with the water, causing it to fall under gravity.  However, if the water droplets are too large, then the airborne dust particles are just moved around, resulting in very little dust being removed. To effectively remove the dust, the water droplets and dust particles must be the same size. Hence, the design of the spray head is of great importance. With preventative suppression, the size of the particle is less important.

Best Practices for Dust Suppression in Underground Coal Mines - Water droplet size effect on dust suppression - Parker Hannifin

 

Dust suppression in Columbia | case study

Parker Conflow, a leader in the industry, works continuously with mining companies and equipment manufacturers to enhance products for preventative dust suppression. In one case, at CI Milpa in Colombia, a manufacturer of metallurgical coal, Parker Conflow engineers designed two dust suppression systems for a mine as well as a fire suppression system on a roadway. 

“We are focused on continually improving the efficiency and safety of our production sites and the Parker Conflow systems are an important part of this. We chose to work with Parker Conflow, because of the company’s expertise in the manufacture and installation of dust and fire suppression systems and are very pleased with the result.”
— David Fernando Jaimes Mojica, CI Milpa

 

Conclusion

Preventive coal dust suppression is vital to ensuring the health and safety of workers and protecting mining equipment from costly downtime and failure. For over 60 years, Parker Conflow has been providing dust suppression, fire suppression and water control equipment and services that help protect workers in the coal mining industry worldwide.

 

Parker purpose

After more than a century of experience serving our customers, Parker is often called to the table for the collaborations that help to solve the most complex engineering challenges. We help them bring their ideas to light. We are a trusted partner, working alongside our customers to enable technology breakthroughs that change the world for the better. 

 

Best Practices for Dust Suppression in Underground Coal Mines - Download the white paper, Science of Coal Dust Suppression - Parker HannifinFor technical details and additional information on preventative dust suppression, download the full white paper “The Science of Coal Dust Suppression”. 

 

Best Practices for Dust Suppression in Underground Coal Mines - Gary Wain Product Manager - Parker ConflowThis blog was contributed by Gary Wain, product manager, Parker Conflow.

 

 

 

 

 

Related content

Defining Our Unique Contribution to the World

Digging Deeper: The Importance of Safety and Reliability in Underground Mining

The Importance of Effective Dust Suppression in Quarries. Part 1

The Importance of Effective Dust Suppression in Quarries. Part 2

Four Ways to Use Hose in a Wet Method Silica Dust Suppression System

OSHA Rule Limits Silica Dust Exposure

Best Practices for Dust Suppression in Underground Coal Mines

2 Jul 2020

Read more

View All
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
      • Parker IPS Design Center Community
    • Filtration
    • Fluid and Gas Handling
    • Hydraulics
    • IoT
      • Mobile IoT
    • Pneumatics
    • Process Control
    • Sealing and Shielding
  • Home
  • All Blogs
  • Home
  • Process Control Blog
  • Process Control Forums
  • Process Control Knowledge Base
  • Process Control Members
  • Mentions
  • Tags
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
Parker - Engineering Your Success
  • Site Map
  • Safety
  • Privacy Policies
  • Terms and Conditions
Ā© Parker Hannifin Corp 2021