Home Technologies Sealing and Shielding Sealing and Shielding Knowledge Base FAQ - Rotary Seals
Sealing and Shielding
  • Technologies
  • More
Sealing and Shielding
Sealing and Shielding Knowledge Base FAQ - Rotary Seals
  • Blogs
  • Forum
  • Knowledge Base
  • Members
  • Sub Groups
  • More
  • Cancel
  • New
Sealing and Shielding requires membership for participation - click to join
  • Sealing and Shielding Knowledge Base
  • FAQ - Back-up Rings+
  • FAQ - Custom Seals+
  • FAQ - Electromagnetic Interference (EMI) Shielding+
  • FAQ - Extreme Temperature Sealing+
  • FAQ - Extruded Profiles & Seals+
  • FAQ - Fastener Seals+
  • FAQ - Gaskets+
  • FAQ - Metal Seals+
  • FAQ - O-Rings & O-Ring Accessories+
  • FAQ - Rotary Seals-
    • Does Parker offer a split oil seal that can be used to retrofit a gearbox in the field?
    • Is a cover plate required to retain Clipper seals since they do not have a metal shell?
    • Which way should we installs the seals?
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
FAQ - Rotary Seals

Print Friendly and PDF

Rotary seals separate system pressures and media against the atmosphere under rotating movements of the opposing surface. There are two generic categories of rotary seals: high-pressure/low-velocity (rotor seals) and low-pressure/high-velocity (rotary shaft seals). Parker provides both symmetrical and unsymmetrical designs.

ss 6/4/2020

  • Does Parker offer a split oil seal that can be used to retrofit a gearbox in the field?
  • Is a cover plate required to retain Clipper seals since they do not have a metal shell?
  • Which way should we installs the seals?
  • rotary seals
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply